A good example is the Cable Lashing Bar. This simple yet innovative solution allows cable bundles to more easily and effectively be anchored back into the depths of the cable manager. When trying to maximize cable capacity, the effective utilization of the interior of the vertical management space is critical. Historically, threading Velcro in order to properly lash cable bundles to the midsection of a cable manager was tedious, time-consuming, and sometimes required a helper on the other side of the row of racks. The Cable Lashing Bar makes this a quick and simple one person job – easy to do from one side while you are installing cable.
One of the favorite innovations delivered with Evolution is the Movable Mid-Section. Since the beginning of time, double-sided vertical cable managers have forced everyone to accept the 50/50 split between front and rear cable management space. But real-world applications rarely need the same space front and rear, so Evolution was designed to allow the Movable Mid-Section to be relocated in the field from the factory default 50/50 location to either a 40/60 or 60/40 split between front and rear area. This is flexibility that has real meaning.
CPI has been driving the evolution of cable management and the next generation is here. Evolution is a great looking product, but the strength of its features are what make it really attractive.
Brian Donowho, Senior Product Manager
|