Logo
Login | Why Login?


Views & Tips

 

CPI’s commitment to excellence begins with quality design and manufacturing and continues with quality service and support. CPI's highly trained customer service and technical support teams provide a level of assistance that is recognized as the industry benchmark.

Views
Find out industry news including the latest trends, solutions and standards updates.

Tips
Take advantage of the collective knowledge of CPI's highly trained Technical Services Group. This group is a combination of Technical Support Specialists and Design Engineers who go the extra mile to make sure you are delighted with the product itself, as well as installation and user experience. Additionally, we are proud that our company has several RCDD-certified employees.

We hope this information will be helpful in organizing, storing and securing your technology equipment. If you have any questions please contact us at techsupport@chatsworth.com or 800-834-4969.

 

Tech Support Tips 

 

 

 

 

 

 

 

 

 

 

 





VIEWS:

 

 

Hot Aisle/Cold Aisle Layout

Today's IT infrastructure equipment is becoming more powerful and compact, resulting in additional heat per enclosure. As more heat becomes concentrated within the cabinet space the risk of overheating and damaging expensive equipment increases. For this reason it is critical to control airflow throughout the data center in efforts to achieve successful cooling. Contemporary thinking in data center thermal management promotes the hot aisle/cold aisle layout where cold air is segregated in front of equipment cabinets and hot exhaust air is expelled behind equipment cabinets. This layout eliminates the direct transfer of hot exhaust air from one system into the intake air of another system.

Cabinets should be arranged in rows that are parallel to airflow creating a hot aisle/cold aisle layout. To begin this type of layout hot and cold aisles must first be designated. The fronts of equipment should face the cold aisles as cold air is delivered to these aisles. There should be perforated floor tiles in the cold aisle that enable cool air to come up from the access floor. The hot aisles should be located behind cabinets as hot air is removed from these aisles; no perforated tiles are located in this area. Whenever possible, utilize overhead cable runway for distributing data and/or power cables. By managing cables above cabinet rows, the under floor space is open and offers greater airflow control and prevents airflow obstruction from cables.

CPI offers a variety of products that help achieve an effective hot aisle/cold aisle layout including the new TeraFrame™ Cabinet System. The TeraFrame Cabinet eliminates internal recirculation, preventing hot exhaust air from entering your equipment. The Internal Air Duct also supplements the cold aisle with an additional 210-510 CFM of cool air, effectively reducing equipment intake air temperature as much as 10ºF (6ºC) over the typical server cabinet. The KoldLok® Raised Floor Grommet blocks airflow through cable access holes in access floor tiles, saving cool air that would otherwise be wasted. Combine CPI's Air Dam Kit, Snap-In Filler Panels, side panels and perforated doors for maximum effectiveness in a hot aisle/cold aisle layout.



TIPS:

Tech Tips

Tech Tip #1
Did I install my CPI Runway correctly?
How do I attach runway to a wall that is not 90 degrees to the runway?

Tech Tip #2
What is the easiest way to install my Vertical Exhaust Duct?

Tech Tip #3
How do you install a Fan Kit in CPI’s MegaFrame®, SlimFrame™, SteelFrame and Seismic Frame Cabinets?

 


Ask Dr. D. Bunk
Got questions about keeping your data center cool?

Ask CPI's Cooling Expert, Dr. D. Bunk!

Myth #1
To achieve 20 kW of cooling you must use liquid or active cooling systems in or near your cabinet.

Myth #2
Cooling units should be located around the perimeter of the data center.

Myth #3
It doesn't matter about the size of a cable cut out hole as long as your cable fits through it.

Myth #4
You cannot use fans in a tier 3 or tier 4 data center.

Myth #5
Water cooled cabinets have little effect on data center design.

Myth #6
It is normal for solid side panels to create extremely hot rows.

Myth #7
You can plan your heat loads from the equipment faceplate ratings.

Myth #8
Super high flow server cabinet doors can't handle C-7000 blade servers.

Myth #9
Fire proof products must be used to fill gaps in a data center.

 

HomeAbout UsProductseCatalogApplicationsNews/EventsSupportPartners

© Chatsworth Products, Inc. |  Privacy PolicyWebmasterContact Us
Home Page About Us Products Catalog Applications News & Events Support Partners