Technical Support 800-834-4969

RMU Placement Logic

close

 

 RMU Placement Logic

When placing accessories in the cabinet, the appropriate number of RMU's will be occupied .  As a rule, the Rack Mounting Units will be measured from the top, or working surface, of the accessory to the furtherest part of the accessory.  From the drawing above, the RMU 's may be measured up, or down, depending on the type of accessory.  This becomes more important when placing a number of accessories close together.  Also, when placing an accessory near the bottom of a cabinet, it is necessary to move the accessory up enough to allow all the RMU 's to fit below. 

 

 Typical Cabinet with Installed Accessories

Accessory Installation Suggestions

 Default RMU locations

The quick rule is to place heavier equipment lower in the cabinet.  This not only helps keep the cabinet more stable but it also makes for easier access to heavy servers when troubleshooting.

Starting at the bottom of the cabinet would be the UPS and tower type servers and above that would be multiple RMU rackmount equipment like servers and switches.  If any of the large equipment is on sliding rails or sliding shelves, then the cabinet stabilizer kit should considered.

Next, is a good place for a locking drawer to store back-up tapes, patch cords and test equipment.  The next area is about mid-height in a 7' cabinet.  This is a logical place to locate a keyboard and shelf for comfortable use.  Just above that would go a monitor shelf. 

Further up would go small switches, patch panels and horizontal wire managers.  The horizontal managers are typically placed above, below, and between patch panels.  Up near the top, is a good location for single sided shelves to support small equipment like tape drives, modems, and KVM switchboxes.

If you are not sure which shelf would be best for your equipment, you can see our shelves in more detail in our eCatalog or contact Technical Support.