Technical Support 800-834-4969

Foam Gasket Kit

close

In certain applications, the air gap between the floor and the bottom of the cabinet may need to be sealed to prevent air loss. It is also beneficial to seal the front of the cabinet from the rear to prevent heated air from mixing with cooled air. These foam pieces, in addition to CPI’s Filler Panels (P/N 30026) creates a cold air chimney along the front of the equipment, assuring delivery of the coldest air where it is most needed. 

 

Twelve 2” x 3” x 40” foam pieces per kit that can be cut to fit 

Foam Gasket Kit