| Chatsworth Products

 

Use side panels to cover the sides of cabinets, secure equipment, and help control airflow.

Solid Side Panels 

Secure equipment in the cabinet and keep hot air from flowing between bayed cabinets. Side panels have locking spring-loaded latches that are recessed into the panel so that the cabinet can be bayed when side panels are installed.  Note, one or two solid side panels are required when using the Vertical Exhaust Duct System.   

35060 Solid Side Panels

 

Vented Side Panels 

Secure equipment in the cabinet and allow air to enter the side of the cabinet. The Vented Side Panel has two large vented openings and includes locking spring-loaded latches that are recessed into the panel so that cabinets can be bayed when side panels are installed.  

35065 Vented Side Panels

 
1/19/2018 8:53:25 PM