Technical Support 800-834-4969

Rear Latches

close

Slam Latch Single Point Latch

Doors with this latch have a swing handle with a keyed lock. The latch is opened (unlatched) by turning the handle, but is closed (latched) simply by shutting the door. There is a single latch point at the midpoint of the door next to the handle. Note that the swing handle has an open and closed position, also, and only turns in the open position. The included keys release the swing handle so that it can be turned.  This type latch cannot be used on double doors.

Swing Handle Single Point Latch

Doors with this latch have a swing handle with a keyed lock. The door is opened (unlatched) and closed (latched) by turning the handle. There is a single latch point at the midpoint of the door next to the handle. Note that the swing handle has an open and closed position, also, and only turns in the open position. The included keys release the swing handle so that it can be turned.
This type latch cannot be used on double doors.

Swing Handle Two Point Latch

Doors with this latch have a swing handle with a keyed lock. The door is opened (unlatched) and closed (latched) by turning the handle. There are two latch points located at the top and bottom of the door. Note that the swing handle has an open and closed position, also, and only turns in the open position. The included keys release the swing handle so that it can be turned.

Swing Latch

 

Combination Lock Single Point Latch

Doors with this latch have a swing handle with a built-in combination lock. The door is opened (unlatched) and closed (latched) by turning the handle. There is a single latch point at the midpoint of the door next to the handle. Note that the swing handle has an open and closed position, also, and only turns when in the open position. The included keys or the pre-programmed combination release the swing handle so that it can be turned. The combination is entered by turning three dials on the handle.  This type latch cannot be used on double doors.

Combination Lock Two Point Latch

Doors with this latch have a swing handle with a built-in combination lock. The door is opened (unlatched) and closed (latched) by turning the handle. There are two latch points located at the top and bottom of the door. Note that the swing handle has an open and closed position, also, and only turns when in the open position. The included keys or the pre-programmed combination release the swing handle so that it can be turned. The combination is entered by turning three dials on the handle.

Combination Slam Latch Single Point Latch

Doors with this latch have a swing handle with a built-in combination lock.  The door is opened (unlatched) by turning the handle but is closed (latched) simply by shutting the door. There is a single latch point at the midpoint of the door next to the handle. Note that the swing handle has an open and closed position, also, and only turns when in the open position. The included keys or the pre-programmed combination release the swing handle so that it can be turned. The combination is entered by turning three dials on the handle.  This type latch cannot be used on double doors.

Combination Latch

 

Electronic Keypad Standalone Single Point Latch

Doors with this latch have a swing handle with an integrated electronic keypad on the front door that controls access to both the front and rear doors. Enter a four-digit to six-digit code on the keypad to release each handle so that it can be turned. The door is opened (unlatched) and closed (latched) by turning the handle. There is a single latch point at the midpoint of the door next to the handle. Each handle can be programmed with ten entry codes (five front/five rear). Programming is done on the keypad using an assigned master code. This latch requires a power connection.    This type latch cannot be used on double doors.

Electronic Latch

Latch Selection Policy

The latches are sold in pairs (as long as the cabinet has two doors). The front latch selection and the rear door style define the rear latch style. 

Front Door Latch Style

Rear Door Style

Rear Door Latch Style

SL1 Slam Latch, single-point latch Single Rear Door SL1 Slam Latch, single-point latch
SL1 Slam Latch, single-point latch Double Rear Door SH2 Swing Handle, two-point latch
SH1 Swing Handle, single-point latch Single Rear Door SH1 Swing Handle, single-point latch
SH1 Swing Handle, single-point latch Double Rear Door SH2 Swing Handle, two-point latch
SH2 Swing Handle, two-point latch Single Rear Door SH2 Swing Handle, two-point latch
SH2 Swing Handle, two-point latch Double Rear Door SH2 Swing Handle, two-point latch
CL1 Combination Latch,
single-point latch
Single Rear Door CL1 Combination Latch,
single-point latch
CL1 Combination Latch,
single-point latch
Double Rear Door CL2 Combination Latch, two-point latch
CL2 Combination Latch, two-point latch Single Rear Door CL2 Combination Latch, two-point latch
CL2 Combination Latch, two-point latch Double Rear Door CL2 Combination Latch, two-point latch
CLS1 Combination Slam Latch,
single-point latch
Single Rear Door CLS1 Combination Slam Latch,
single-point latch
CLS1 Combination Slam Latch,
single-point latch
Double Rear Door CL2 Combination Latch, two-point latch
EKS Electronic Keypad, Non-networkable, single-point latch Single Rear Door EKS Electronic Keypad, Non-networkable, single-point latch
EKS Electronic Keypad, Non-networkable, single-point latch Double Rear Door Not available for double doors