| Chatsworth Products

Mission Critical & Data Center Expo

When: Wednesday, February 11, 2015 4:55 PM - 6:30 PM

Where: Atlanta, GA


Steven Bornfield, CPI Senior Data Center Consultant, will be speaking at the Mission Critical & Data Center Expo in February.

His presentation is titled "Orlando Health - High Rise Data Center"

Presentation Summary: Orlando Health wanted to construct a new data center because of hot spot issues in its original data center. With CPI’s solutions and expertise, the space now uses less than 2/3 cooling capacity to cool 200% of the original IT load. Over $350K was saved by reusing older CRAC units, and $120K was saved by not using a raised floor. Cabinet-supported fiber duct and low-voltage basket trays also saved $350 per cabinet installation cost. 

Find out more at: http://mcdcexpo.com/ 

3/18/2018 4:56:06 AM