New Online Estimator Delivers Personal Report of Savings from IP Consolidation | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X

New Online Estimator Delivers Personal Report of Savings from IP Consolidation

 Intuitive Tool Provides Detailed Report of Dollars Saved using Secure Array™ over Traditional Network Deployments When Instrumenting Data Center Cabinets

Secure-Array-EstimatorAGOURA HILLS, Calif., Nov. 14, 2017 — Customers can now easily understand the cost savings of deploying Secure Array™ IP consolidation technology thanks to a new online estimator introduced by Chatsworth Products (CPI), the leader in data center infrastructure.

The cost of instrumenting cabinets in the data center can be significantly high because of the number of additional network ports and IP addresses needed to network sensors. Traditional networks typically require one connection for each PDU, environmental appliance and electronic access control system per cabinet.

Secure Array, an award-winning eConnect feature, reduces costs and decreases installation time by allowing customers to link up to 32 eConnect PDUs under a single IP address using standard Ethernet cables. Additional features include outlet grouping, data logging, threshold alarms and PDU cloning. Adding a second IP address provides failover capability, which allows functioning PDUs to continue communicating if a PDU in the array loses connectivity.

Because eConnect PDUs seamlessly integrate with environmental monitoring and eConnect Electronic Access Control (EAC), 16 cabinets can be fully instrumented using only two connections instead of traditional deployments that require up to four network connections per cabinet. The online estimator demonstrates this substantial cost benefit.

Based on entered information such as number of cabinets, cost of network port and types of appliances used, the Secure Array Savings Estimator tool creates a comparison report between Secure Array and traditional network deployments, as well as total savings in dollar amount. 

Additional information provided by the tool include:

  • Number of cabinets
  • Cost of each port
  • Number of connections needed
  • Cost of connections needed
  • Number of unused connections
  • Cost of unused connections

To learn more about the Secure Array Savings Estimator tool, click here. For more information about CPI’s eConnect product line, visit the product page.

About Chatsworth Products 
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.

CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).

More Information
www.chatsworth.com
info@chatsworth.com
800-834-4969

Media Contact
Raissa Carey
Public Relations 
rcarey@chatsworth.com
512-591-9525

©2018 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, Motive, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. 
9/24/2018 7:46:00 PM