Chatsworth Products Patent-Pending Clik-Nut™ Hardware Kit Now Included with Select Cabinet Systems | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X

Chatsworth Products' Patent-Pending Clik-Nut Hardware Kit Now Included with Select Cabinet Systems
Innovative, Tool-less Cage Nut Reduces Labor and Installation Time by at Least 70%

AGOURA HILLS, Calif., August 21, 2017 — Customers can now purchase Chatsworth Products’ (CPI) popular F-Series TeraFrame® and GF-Series GlobalFrame® Cabinet Systems with Clik-Nut Hardware Kit included, which reduces installation time by at least 70 percent.Clik-Nut Hardware Kit

Clik-Nut is a tool-less cage nut, which features a patent-pending squeeze-and-release design—eliminating the need for tools. Clik-Nut provides the same strength and reliability as standard cage nuts and is fully compatible with square-punched holes.

Standard cage nuts can be difficult and time-consuming to install and move, requiring force that exceeds what can be reasonably applied by human fingers. Consequently, installers routinely suffer from pinched fingers, ripped or detached fingernails. CPI’s Clik-Nut Hardware Kit solves these issues.

“Anyone who has ever used cage nuts will attest they are not easy to install or remove. They are difficult and painful to install without a specialty tool; the tool is always missing when you need it, and no tool works well for both installation and removal. The increasing number of requests to install these at the factory combined with general customer comments over the years motivated us to take a second look,” stated Sam Rodriguez, CPI Sr. Product Manager of Cabinet & Thermal Solutions.

Advantages of Clik-Nut include:

  • No tools required – squeeze-and-release design allows for easier, faster and safer installation
  • High payload capacity – same strength and reliability as standard cage nuts
  • Universal usability – fully compatible with .375” (9.5 mm) EIA square-punched holes

Users must simply align the Clik-Nut with the desired mounting hole, squeeze and release the tab. The Clik-Nut will then be fastened in place and ready for equipment mounting.

“I am confident that our customers will be pleased. Instead of creating a better tool, we eliminated it. The end result is a fast, safe and simple design that provides the same high reliability attachment the industry has relied upon for decades,” Rodriguez added.

Order your cabinet with Clik-Nut today, or purchase Clik-Nut separately. For more information about this product, watch the video.

 

About Chatsworth Products 
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.

CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).

More Information
www.chatsworth.com
info@chatsworth.com
800-834-4969

Media Contact
Raissa Carey
Public Relations 
rcarey@chatsworth.com
512-591-9525

©2018 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, Motive, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. 
5/25/2018 12:01:14 AM