| Chatsworth Products
We use cookies to personalize content and to analyze our traffic. We do not share information about your use of our site. You consent to cookies if you continue to use this website. X

CPI Adds New Features, Improves Design of its Two-Post Standard Rack


Two-Post Standard Rack with Integrated GroundingWESTLAKE VILLAGE, California, US – September 2013 - Chatsworth Products (CPI) has enhanced its popular Two-Post Standard Rack, otherwise known as “THE Rack” or “55053,” the product customers ask for by number.

The industry-leading Standard Rack is a high quality, cost-effective storage solution for patch panels and network switches. The rack features a small footprint, making it the best choice in many telecommunications and equipment rooms where floor space is limited.

Made from aluminum extrusion, the Standard Rack features unmatched sturdiness and durability. A convenient element is the rack’s 19” EIA universal rail spacing with marked and numbered U spaces. It is available in three heights: 7 feet (2.1 m), 8 feet (2.5 m) and 9 feet (2.7 m). The heavy-duty rack is UL Listed with up to 1,000 lb. (454 kg) weight capacity.

The new features added to CPI’s Standard Rack include: 

  • Grounding and Bonding with integrated ground studs
  • Rack Ground Jumper Kit (ordered separately) 
  • 52U height on 8’H racks
  • Glacier White finish

Now with 52 rack units and bonded assembly, the Standard Rack has a prepared grounding location added to one side of the rack channel. The Rack Ground Jumper Kit (ordered separately) allows for quick and easy attachment to the Telecommunications Grounding System, thus reducing installation labor.

Michael Moore, CPI’s Product Manager of Open Architecture, stated, “CPI’s new integrated grounding features included with the Standard Rack ensure proper grounding and bonding, as well as reduction in labor time. This new design does not use any RMU space in the rack footprint, which in return saves money and allows full utilization for equipment.”

It is now available in Glacier White, which is a new standard CPI color. Glacier White finish is highly reflective and helps brighten narrow equipment rows, provide better visibility and reduce energy costs.

For more information about the updates made to CPI’s Standard Rack, visit our Two-Post Rack web page.

About Chatsworth Products 
At Chatsworth Products (CPI), it is our mission to address today’s critical IT infrastructure needs with products and services that protect your ever-growing investment in information and communication technology. We act as your business partner and are uniquely prepared to respond to your specific requirements with global availability and rapid product customization that will give you a competitive advantage. At CPI, our passion works for you. With over two decades of engineering innovative IT physical layer solutions for the Fortune 500 and multinational corporations, CPI can respond to your business requirements with unequaled application expertise, customer service and technical support, as well as a global network of industry-leading distributors. Headquartered in the United States, CPI operates from multiple sites worldwide, including offices in Mexico, Canada, China, the United Arab Emirates and the United Kingdom. CPI’s manufacturing facilities are located in the United States, Asia and Europe.

CPI is listed with the General Services Administration (GSA) under Federal Supply Schedule IT 70. Products are also available through GSA Advantage and through Government Wide Acquisition Contracts (GWACs), including GSA Connections and NITAAC-ECS III (www.chatsworth.com/gov).

More Information
www.chatsworth.com
info@chatsworth.com
800-834-4969

Media Contact
Raissa Carey
Public Relations 
rcarey@chatsworth.com
512-591-9525

©2018 Chatsworth Products, Inc. All rights reserved. Chatsworth Products, Clik-Nut, CPI, CPI Passive Cooling, Secure Array, eConnect, Evolution, GlobalFrame, MegaFrame, OnTrac, QuadraRack, RMR, Saf-T-Grip, SeismicFrame, SlimFrame, TeraFrame and Velocity are federally registered trademarks of Chatsworth Products. EuroFrame, Motive, CUBE-iT and Simply Efficient are trademarks of Chatsworth Products. All other trademarks belong to their respective companies. 
4/23/2018 4:15:18 PM