First on the list, stop by and see us in booth 213 to get a firsthand look at the latest CPI technologies and products. Then, be sure and add these to your agenda:
Join CPI on Wednesday, Feb. 7 from 1:30 – 2:30 p.m. for a presentation titled, “Remote Management of Data Center White Space: What to Manage and How.” CPI expert and senior product manager, Ashish Moondra, discusses the need for white space management, and initiatives and solutions that can help optimize data center efficiency, security and safety.
As a sponsor of BICSI’s Cabling Skills Challenge, CPI invites you to witness our products in action. Competitors will participate in eight cabling skills events race against their peers—and the clock—to win $5,000 and become BICSI’s 2018 BICSI Installer of the Year.
CPI products being used in the Cabling Skills Challenge include:
Standard Rack provides support of equipment and cabling in cost-sensitive or general applications. Integrated grounding with a built-in attachment point for a ground (earthing) connection and is available in three heights and three widths.
MCS Master Cabling Section is a heavy-duty system for major installations. It virtually eliminates the need for horizontal cable managers by providing frequent 1U spacing of the cable guides that aligned precisely with the rack spacing.
Universal Cable Runway supports backbone and horizontal cables between the point of entry and exit into the telecommunications or equipment rooms, and cross-connects on racks or cabinets with other CPI Cable Runway Products.
Universal Horizontal Cable Manager creates an attractive and highly functional horizontal pathway for patch cords and multimedia applications using coax, copper and fiber optic cables. After routing the cables or cords, simply snap on the cover for a clean, professional appearance.
Be sure to make a stop by booth 213 to visit with our staff and see the latest CPI technologies and products, including:
Newly Redesigned CUBE-iT™ Wall-Mount Cabinet
Get a sneak-peak at the newly redesigned, soon-to-be released CUBE-iT-Wall Mount Cabinet. Updated features to note include the ultra-quiet fan, internal latch for rear access, increased load rating and new front door with tempered glass window.
RMR® Industrial Enclosures
RMR® Industrial Enclosures provide solutions engineered specifically for technology, automation and control equipment in harsh indoor and outdoor environments.
Motive™ Cable Manager
Motive™ Cable Manager is a highly intuitive and sophisticated cable manager that includes a set of tool-less accessories to provide unlimited adjustability and direct support for cable bundles, while maximizing use of interior space.
eConnect® Power Distribution Units (PDUs)
eConnect® PDUs provide the ultimate solution for cabinet-level power distribution. With innovative capabilities such as patented Click Secure Technology, Secure Array™ IP Consolidation and the ability to ship preinstalled in CPI cabinets, eConnect PDUs offer the quickest and lowest cost deployment among all intelligent rack PDU solutions in the industry.
F-Series TeraFrame® Gen 3 Cabinet System
The F-Series TeraFrame® Gen 3 Cabinet System is a highly configurable premium enclosure that provide exceptional thermal and cable management. Perfect for high-performance server and network applications.
Clik-Nut® Hardware Kit
Clik-Nut® Hardware Kit is a tool-less cage nut that features a squeeze-and-release design, reducing labor and installation time by at least 70%. Clik-Nut's price has been reduced. Stop by and order a free sample.
Learn more or register for the event by visiting the website. If you can’t attend, schedule a visit to our office or showroom where you can interact with our products and discuss your toughest ICT challenge with one of our data center infrastructure management experts.
Brittany Mangan, Digital Content Manager