Cross-Connect Blog

Norway-Based SpareBank 1 Achieves Lower PUE with CPI Hot Aisle Containment

August 06, 2015

Sparebank 1 - SPAREBANK_CONTAINMENT_DOOR_RGB72.jpgSpareBank 1, a Norway-based alliance of banking organizations was able to improve its data center infrastructure and lower its Power Usage Effectiveness (PUE) with Chatsworth Products’ (CPI) flexible and innovative data center solutions.

SpareBank 1 wanted a state-of-the-art data center specifically tailored to its organizational needs. Additionally, they needed a solution that would fit into the existing environment and accommodate 200 kW of power and cooling to maintain the continuity of operations.

To meet this unique installation requirement and to create the most efficient solution possible, SpareBank 1 selected CPI’s Hot Aisle Containment (HAC) Solution, Two- and Four-Post Racks, Evolution® Cable Management and Accessories. CPI’s HAC Solution completely isolates hot exhaust air from IT equipment and removes it from the room, resulting in more efficient cooling units. More importantly, it helped the alliance achieve its desired PUE goal of 1.3.

“For the design of the solution, I like the interoperability of CPI products. I can pick and choose and assemble a solution,” stated Magnus Askautrud, Business Development Manager for Coromatic.

Click here to read the full case study.

CPI's German Manufacturing Location Benefits European Customers 

Additionally, to better serve the increasing demands of global and local customers, such as SpareBank 1, CPI has increased its European production capabilities by setting up a manufacturing location in Ellwangen, Germany.

At this prime location, CPI will manufacture the TeraFrame® and GlobalFrame® family of cabinets, as well as accessories. A product showroom has also been created and will be open to customers and channel partners in the region.

For more information, contact a local CPI Sales Representative.

Shannon Erdley, Public Relations Specialist

Search CPI in the News