UK-Based Aviation Company's Communications Room Redesign Results in Savings | Chatsworth Products
 

UK-Based Aviation Company's Communications Room Redesign Results in Savings

(Applications, Data Center, International, Thermal Management) Permanent link


Menzies Aviation Case Study - MENZIES_STAFF_RGB72.jpgMenzies Aviation, a leading global provider of passenger, ramp and cargo services in the United Kingdom, stored all of its important and confidential information in a communications room that needed reconstruction to optimize airflow and improve cooling inefficiencies. 

Challenge
The main challenge in Menzies Aviation’s communications room was the low plenum ceilings. In some instances, structural beams passed a mere 300 mm above the tops of cabinets. The beams supported trusses, so there was sufficient space for airflow above the finished ceiling plenum, but the space between the tops of the cabinets and the finished ceiling was limited.

This affected Menzies Aviation’s ability to regulate air efficiently, so they needed to deploy an effective cabinet and duct solution to maintain a standard volume but fit in the restricted overhead space.

Solution
Menzies Aviation partnered with Impact Data Solutions (IDS), a designer and installer of IT equipment, to help remodel the communications room. After assessing the needs of the communications room, IDS professionals recommended using passive cooling technology, making Chatsworth Products (CPI), the pioneers of Passive Cooling® Solutions, the best choice for the project.

Menzies Aviation Case Study - MENZIES_VED_RGB72.jpgProducts Used
To accommodate the limitations of the building’s design and the low plenum ceiling in the communications room, CPI designed custom GF-Series GlobalFrame® Cabinets with Vertical Exhaust Ducts, split rear doors, solid side panels and vented front doors.

With this solution, Menzies Aviation was able to maximize its cooling efficiencies without the need for additional CRAC units, in-row air conditioners or liquid cooling solutions.

Now Menzies Aviation’s server room is running on free air cooling, and they are looking to achieve better efficiencies, while increasing their infrastructure footprint with ease. 

"Working closely with the CPI team enabled us to fine tune a small delivery window, which was essential in the success of this project."
- Robbie Williams, CEO Director of IDS 

Visit CPI's Case Study library for the complete story and additional photos, or take a look at other installations.

Kim Ream, Marketing Project Manager


Posted by Kim Ream, Marketing Project Manager at 01/06/2015 08:21:45 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email techsupport@chatsworth.com for assistance with these matters.


2/18/2018 2:47:11 AM