Tech Tip: When Should I Use Adjustable Cable Runway Instead of Traditional Runway? | Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

Tech Tip: When Should I Use Adjustable Cable Runway Instead of Traditional Runway?

(Cable Management, Tech Tips, Cable Pathway) Permanent link

Adjustable Cable Runway Tool-less AccessoryChatsworth Products (CPI) offers traditional and adjustable runway products. Both products are similar in length, width, form and finish. However, CPI’s Adjustable Cable Runway does not have welded cross members. This allows an installer to easily place the cross members (using two thread-forming screws) anywhere along the side stringers to best accommodate cables entering and exiting the runway.

This is especially useful in applications where the runway supports cabling above racks, cabinets and vertical cable managers. Customizing the pathway to address these varied cable drops no longer requires excessive tools and labor. Simply loosen the screws, and slide the cross member into place and tighten. No touch-up paint is needed since Adjustable Cable Runway’s components are painted individually.

To further simplify installation, use CPI’s tool-less radius drops and pathway dividers, which securely attach to the runway without the need for tools.

Many installers use traditional runway in applications where there is no need for unique cable drops, using adjustable runway only where needed. CPI’s Adjustable Cable Runway is fully compatible with CPI’s other runway products.

CPI’s Adjustable Cable Runway supports a load rating of 132 lb/ft (196 kg/m), has a bonded construction and meets ANSI, TIA and EIA for copper and fiber cable guidelines.

Compare CPI’s cable runway using this handy quick reference guide, or download the Adjustable Cable Runway data sheet.

Kim Ream, Marketing Project Manager


Posted by Kim Ream, Marketing Project Manager at 01/17/2017 01:58:37 PM




Comments

What are the requirements for the spacing and quantity of cross-members in order for the tray to satisfy the 132 lb/ft rating?
Posted by: Ryan Standish at 1/18/2017 10:07 AM


Ryan, the load rating is 132 lb/ft (196 kg/m) when the runway is supported every 5 ft (1.5 m). Additionally, CPI Tech Support recommends that the rungs be no more than 12” apart. Please feel free to reach out to our very responsive technical team at techsupport@chatsworth.com.
Posted by: Kim Ream at 1/19/2017 9:12 AM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email techsupport@chatsworth.com for assistance with these matters.


5/21/2018 6:13:18 AM