| Chatsworth Products
We use cookies to personalize content and to analyze our traffic. You consent to cookies if you continue to use this website. To find out more or to disable cookies view our Privacy Policy. X
 

KoldLok Mini Raised Floor Grommet Helps Increase Data Center Cooling Efficency

October 23, 2008

CPI now offers the KoldLok® Mini Raised Floor Grommet, which seals cable holes in access floor tiles as small as 4” x 6” without damaging cables. The patent pending KoldLok Mini is made with fire rated resin and filaments that meet

F-Series TeraFrame™ Cabinet: Selecting the Right Top Panel Can Expand Future Options

October 17, 2008

Four is the new one With the recent release of the new telescoping Vertical Exhaust Duct System for the F Series TeraFrame™ Cabinet there was a change made to the cabinet’s Server Top Panel. It was redesigned to support the

Intel Uses CPI Products in One of the Highest Density Data Centers in the World

October 09, 2008

Is it possible to efficiently cool 4,700 blade servers that are generating 30 kW of heat per rack on a slab floor? According to Intel, that is exactly what they are doing using CPI Passive Cooling® Solutions. Intel recently released

What Is New, What Does It Do?

October 03, 2008

Industry conferences and tradeshows seem to be one of the best opportunities to get a firsthand look at new products and solutions. The BICSI Fall Conference held in Las Vegas earlier this week gave CPI the opportunity to introduce several

FirstPrevious1NextLast
6/19/2018 9:06:05 PM