Tech Tip: What is the difference between an Evolution g1 Single-Sided, and Evolution g2 Double-Sided and an Evolution g3 Combination Vertical Cable Manager? | Chatsworth Products
 

Tech Tip: What is the Difference Between an Evolution® g1 Single-Sided, Evolution g2 Double-Sided and an Evolution g3 Combination Vertical Cable Manager?

(Cable Management) Permanent link

 

Chatsworth Products’ (CPI) Evolution Vertical Cable Management is designed for larger, heavier cables such as the Cat 6a UTP. 

Evolution g1 Single-Sided Cable Manager

  • It has plastic T-shaped cable guides (fingers) only on the front and a door.  
  • It is used to support and manage large bundles of cable on the front of the rack. 
  • Used on Two-Post or Four-Post Racks into the horizontal manger or into the equipment.

Evolution g2 Double-Sided Cable Manager

  • It has the T-shaped fingers on the front and rear, and includes a curved front door and a flat rear door. 
  • The internal mid-sections can be moved to create 40/60 50/50 or 60/40 front/rear split of the internal cable management space.
  • Also supports and manages large bundles of cable on the rear of the rack.
  • Used on Two-Post or Four-Post Racks into the horizontal manger or into the equipment

Evolution g3 Combination Cable Manager

  • It combines a single-sided vertical cable manager on the front side and multiple large, open cable rings on the back side. 
  • With rings located on the front and rear of the manger, it allows for large bundles of cables to be supported on the rear and for patching cables on the front.
  • Used on Two-Post or Four-Post Racks into the horizontal manger or into the equipment

To see all other valuable features of Evolution Cable Manager, be sure to visit the product page.

Posted by Kim Ream at 05/09/2014 01:34:06 PM


Leave a comment
Name (required)
Email (optional, not published)
Your URL (optional)
Comment


Note: Conversation is encouraged and expected. However, moderation of comments is necessary to prevent spam, personal attacks, profanity, or off-topic commentary. Comments related to specific product support or customer service issues will be addressed separately rather than posted here. Please email techsupport@chatsworth.com for assistance with these matters.


2/22/2018 10:44:54 AM