Cross-Connect Blog

Out with the Cold, in with the New for CPI at Interop Las Vegas 2012

April 23, 2012

It’s a good thing that Chatsworth Products, Inc. (CPI) is skilled at handling high density situations – but we’re not talking fully populated cabinets or racks, we’re navigating an events calendar that’s jam-packed with seminars, office openings, and in this case, the Interop Las Vegas 2012 IT Conference and Expo.

Join CPI at Interop Las Vegas 2012This May 8-10 at Mandalay Bay, we’ll be displaying a new benchmark in data center efficiency at booth 1667, that of CPI’s Aisle Containment Solutions, featuring a neon-lit Hot Aisle Containment configuration complete with four CPI F-Series TeraFrame® Cabinets and a nifty self-closing and sliding door for maximum seal, security and support.

CPI's 2012 Booth Display feat. Aisle ContainmentA look at the CPI booth that will be on display this May 8-10 at Interop 

Hailed as one of the industry’s best annual events, Interop consistently pushes the envelope on cutting-edge technologies such as the cloud, virtualization and mobility, all areas that could see significant operational savings from the use of well-engineered aisle containment.

Ian Seaton, CPI’s Global Technology Manager, points out that “energy required to cool the data center has traditionally constituted 30-50% of the entire data center energy budget… now that data centers are included in ASHRAE 90.1, Energy Standard for Buildings Except Low-Rise Residential Buildings, state energy and building codes will begin prescribing economizers for new data centers or major expansions and upgrades. These major capital expenses can be recouped much more quickly with an intelligent white space design for effective air flow management.”

When you consider that CPI’s Aisle Containment Solutions can increase cooling efficiency by 3x, while broadening the air temperature envelope with 4x higher heat and power densities, the question of implementation becomes when, not if.

With a variety of CPI sales, engineering and technical support on hand during this event, you’ll have no trouble finding the answer. And with this special discount coupon from CPI, you can register today and earn 25 percent off a conference pass or get an expo pass completely free! See you there. Jeff Cihocki, Global eContent Specialist  

Search CPI in the News