Cross-Connect Blog

International Events: Chatsworth Products to Exhibit at BICSI Canada, BICSI Andino

April 13, 2016

BICSIChatsworth Products (CPI) invites you to two international BICSI Conferences in May. Visit Booth 315 at the 2016 BICSI Canadian Conference & Exhibition in Niagara Falls, Ontario, Canada, May 2-5 at the Scotiabank Convention Centre. Or, if you’re down in South America, CPI will be at DataNet Bicsi Andino, in Bogota, Colombia, May 4-5 at Booth 304.

By attending these events, you can gain insight into technologies and local industry trends, as well as network with peers from all over the world. Also, learn about CPI latest releases such as: 

  • eConnect® Power Distribution Units – Now include Click Secure Locking Outlet options to help prevent accidental disconnections. Additionally, Secure Array IP Consolidation™ is now available, allowing the use of a single IP address for up to 32 connected PDUs.
  • Adjustable Cable Runway – Features unique, movable Cross Members, which allow components and accessories to be installed at various points along the runway, simplifying the alignment of cabling above racks, cabinets and cable managers.
  • Two-Post Racks with Cable Management – CPI’s industry-leading Two-Post racks support equipment and cabling with unsurpassed strength, stability and durability.  

At BICSI Andino, Victor Bañuelos, CPI’s Technical Manager, CDCDP™, Uptime Institute Accredited Tier Designer, will discuss the comparison of various data center cooling systems such as Hot Aisle Containment, Cold Aisle Containment and Vertical Exhaust Ducts.

CPI participates in a variety of industry events throughout the globe to share knowledge, present new products and network with customers. Contact our local offices in Mexico and Canada for more information on these events. 

Don’t forget to like and visit our Facebook page to see pictures of the latest shows, including Data Centre World, which is taking place this week in London.

Raissa Carey, eContent Specialist

 

Search CPI in the News