Your Cart (0)

Your cart is empty.

Cart Subtotal:
MSRP (USD)
$0

In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

Specifying Equipment Racks for Seismic Environments

March 17, 2009

The below information was taken from an article in Equipment Protection Magazine, written by Alan Taft, CPI Sr. Product Manager. Download the entire article in PDF format.

On any given day, per the National Earthquake Information Center (NEIC) our earth experiences approximately 25 earthquakes with a magnitude of 2.5 or above on the Richter scale

The highest risk areas within the United States are Hawaii, the entire west coast including the southern region of Alaska, the area around St. Louis, Missouri, the border between Utah, Idaho, Wyoming and Montana and areas around Charleston, South Carolina. Internationally, the west coast of Central and South America, Japan and the islands in the western Pacific Ocean south of Asia and east of Australia, central and western China, the area around Afghanistan, Turkey, Greece and southern Europe are the highest risk areas. Data centers built within these seismically active environments require specialized equipment and racks with special mounting specifications.

The Rack
The commonly accepted standard test to certify compliance of a rack with zone 4 seismic events is defined by Section 4.4, “Earthquake, Office Vibration and Transportation Vibration” of Telcordia® Technologies, Inc. GR-63-CORE Network Equipment Building Systems (NEBS) requirements for Physical Protection. Seismic equipment racks are typically designed to secure 500 pounds (227 kg) with some models available up to 1000 pounds (454 kg) of evenly distributed equipment.

CPI-Seismic-Rack-Deflection-Graph.gif

The chart above is from an actual GR-63-CORE test on a Chatsworth Product, Inc. (CPI) seismic rack (the Seismic Frame® Two-Post Rack). It depicts the amount of rack side-to-side deflection observed over the test period. The maximum deflection allowed per GR-53-CORE is +/- 3.0 inches of rack movement from its original position. The chart shows the actual tested deflection at only 1.0 inch, which is well within the NEBS maximum allowed specifications.

This video shows the above rack being tested.

Installation
It is vitally important that hospitals and critical data centers have equipment that has been seismically rated and installed per the manufacturer’s and Structural Engineers recommendations. It is equally important to ensure that the rack is properly mounted within the particular building. Fasteners and anchors with a high shear and high tensile strength rating should be selected to secure the racks. When mounting to concrete floors it is extremely important to choose seismically rated floor anchors that have been rated to support the load of the rack, equipment and overhead cable pathways.

Download the entire article to get full details on the following key areas:

  • Grounding/Bonding
  • Cable Management and Pathways
  • Adjustability
  • RMU Markings
  • Screws or Cage Nuts
  • Rack Height / Widths
  • Electrical Boxes
  • Shelves / Trays
  • Cable Fingers
  • Vertical Power Strips

CPI's Seismic Frame® Two-Post Rack meets the criteria listed above. If you have comments or questions about the information in this article or seismic concerns, please leave a comment using the “Comment” link below.

Search CPI in the News
Categories
Archives