Your Cart (0)

Your cart is empty.

Cart Subtotal:
MSRP (USD)
$0

In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

F-Series TeraFrame™ Cabinet: Selecting the Right Top Panel Can Expand Future Options

October 17, 2008

With the recent release of the new telescoping Vertical Exhaust Duct System for the F-Series TeraFrame™ Cabinet there was a change made to the cabinet’s Server Top Panel. It was redesigned to support the duct in all 600 and 700 mm wide F-Series TeraFrames that are 1050 mm deep or deeper. All cabinets that are less than 1050 mm deep have the traditional Server Top Panel. The new Server Top Panel allows you to install the Vertical Exhaust Duct by simply removing a pre-cut piece from the top panel and attaching the duct.

Top Panels

This upgrade is reflected in the part number matrix of the F-Series TeraFrame Cabinet. Previously, you would have selected option #1 under the section titled “Top Panel Style”, but now you will need to select option #4.

Top Panel Option

This change in the F-Series part number matrix is not reflected in the current catalog but is available in the online Product Configurator.

Top Panel Option 2

If you want to order a new cabinet without the Vertical Exhaust Duct option but think you may want to add the duct later, then be sure to select a cabinet that is at least 1050 mm deep along with Top Panel option #4. When ordering new TeraFrames, it is a good idea to specify the #4 option because of the upgradeability it offers. For additional information, visit our website or contact Technical Services. John Bennett, Sr. eMarketing Specialist

Search CPI in the News
Categories
Archives