Your Cart (0)

Your cart is empty.

Cart Subtotal:
MSRP (USD)
$0

In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

Snap-In Filler Panels Now Available in Packs of 50

October 13, 2009

Snap-In Filler PanelCPI's popular Snap-In Filler Panels, which is available in both 1U and 2U, are now available in packs of one, six and 50.

Snap-In Filler Panels are solid panels used to fill open rack mounting spaces in cabinets that store rack-mount computer servers and data storage equipment.

Use filler panels in any CPI Cabinet System that is equipped with 19” EIA square-punched equipment mounting rails. No tools or hardware are required for installation. Simply line up the posts on the back of the Snap-In Filler Panels with the square-punched holes in the equipment mounting rails and push – the panels snap in place. To remove, pull on the indented areas on the front edge of the panel – the panel snaps out.

When deploying CPI Passive Cooling® Solutions, use Snap-In Filler Panels in combination with the Air Dam Kit to create an internal airflow barrier between the front and back of the cabinet. The airflow barrier blocks recirculation of hot exhaust air from the back of the cabinet to the front of the cabinet, which keeps cooling air temperatures lower because cold air goes through equipment without being pre-heated by hot exhaust air.

For more information download the Snap-In Filler Panels Data Sheet or email us at techsupport@chatsworth.com. Kim Ream, Sr. eCommerce Specialist

Search CPI in the News
Categories
Archives