Your Cart (0)

Your cart is empty.

Cart Subtotal:
MSRP (USD)
$0

In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

CPI’s Standard Rack Now Has Grounding Features

September 27, 2013


Two-Post Standard Rack with Integrated GroundingChatsworth Products (CPI) has enhanced the design of its industry-leading Two-Post Standard Rack, popularly known as “THE Rack” or “55053.” 

An effective storage solution for patch panels and network switches, the aluminum extrusion rack features unmatched sturdiness and durability. Furthermore, it features a small footprint, making it the best choice in many telecommunications and equipment rooms where floor space is limited. Another convenient element is the rack’s 19” EIA universal rail spacing with marked and numbered U spaces. 

An important feature is that The Rack has now a grounding location added to one side of the rack channel, thus ensuring proper grounding and bonding, as well as reduction of labor time. In addition, the new design does not use any rack mount unit space in the rack footprint, which in return saves money and allows full utilization for equipment.

The Two-Post Standard Rack is now available in Glacier White, a new standard CPI color. Because it’s highly reflective, the finish provides better visibility, thus reducing energy costs. Other attributes include: Grounding and Bonding with integrated ground studs and 52 U on 8’H racks instead of 51. Available in three heights (7 feet, 8 feet and 9 feet), the rack has a new accessory Rack Ground Jumper Kit that can be ordered separately. 


For more information about CPI’s Standard Two-Post Rack, go here.

Raissa Carey, eContent Specialist

Search CPI in the News
Categories
Archives