• About
  • News & Events
  • Partners
  • Contact Us
  • 800.834.4969
Your Cart (0)

Your cart is empty.

Cart Subtotal:
MSRP (USD)
$0

In order to provide complete functionality, this web site needs your explicit consent to store browser cookies. If you don't allow cookies, you may not be able to use certain features of the web site including but not limited to: log in, buy products, see personalized content, switch between site cultures. It is recommended that you allow all cookies.
I hereby accept that the provided information can be used for marketing purposes and targeted website content.

You can find more information on our privacy page.

Be the Superhero of Your Data Center – Here’s How

August 29, 2013


Be Data Center Super Hero Blog

Data managers across the country know this story all too well: Internal CPU temperatures get too hot to operate, proper cooling isn’t achieved and finally the dreaded server failure – or even melting – actually happens.

The good news is Chatsworth Products’ (CPI) Aisle Containment Solutions can help IT professionals and data center managers to become true “superheroes.”

That’s no exaggeration.

It's been determined, between 30 and 50 percent of all data centers will run out of power and cooling within the next year, and an average of four times more cooling will be used than is actually required by the IT load. By using airflow containment, it’s possible to recapture stranded or lost capacity, all while prolonging the life of your data center infrastructure.

To put this into perspective, this could mean between $5-$25 million in savings.

AISLE_CONTAINMENT_HAC_CAB_WHT_RGB72.jpg

For example, CPI’s Cabinet Supported Hot Aisle Containment isolates hot exhaust air from IT equipment in the hot aisle and directs it back to the CRAC/CRAH through a vertical exhaust duct. 

AISLE_CONTAINMENT_FS_HAC_CAB_WHT_RGB72.jpg

Meanwhile, CPI’s Frame Supported Hot Aisle Containment is perfect for colocation facilities and data centers requiring easy roll-in/roll-out capabilities, as it combines self-closing Aisle Containment Double Door Assemblies at each end of the aisle and a Frame Supported Exhaust Duct that features an independent frame that can stand on its own, allowing cabinets with varying heights to be easily added and moved.

AISLE_CONTAINMENT_CAC_CAB_WHT_RGB72.jpg

In addition, CPI developed the Cabinet Supported Cold Aisle Containment, ideal for smaller physical footprint requirements, as it confines cold air supply to an entirely closed off area targeted at cooling IT equipment instead of the room. Custom Aisle Containment Solutions are also available, and our engineers are always ready to work with you to create the best solution for your needs.

By rescuing lost power and cooling with containment, you can defend and extend the life of your data center and become a true Data Center Superhero.

To find out how you can add more computing capacity and gain up to 12 years of extended life out of your data center cooling capacity, read CPI Global Technology Manager, Ian Seaton’s White Paper titled, “Extend the Life of Your Data Center” here.

Raissa Carey, eContent Specialist

Search CPI in the News
Categories
Archives