The Heat is On ... at the Cabinet Level. Attend a Webinar to Find Out How Airflow Containment Can Help.
February 27, 2020
In a reality where cabinet densities are rising—with recent research stating upwards of 10 kW per rack, on
average—increasing energy efficiency and keeping operating costs down in the data center has never been so relevant. It also has never been so challenging. The good news is that redirecting heat through airflow containment doesn't have to be extremely complex. And, there are plenty of cost-effective solutions to consider as you try to stay within budget.
Join Chatsworth Products’ (CPI) Tom Cabral and Critical Environments Groups’ (CEG) Rob Huttemann during a live, complimentary webinar titled, "Rack Densities on the Rise: Why Now Is the Prime Time for Airflow Containment," as they discuss the best practices and benefits of cabinet-level containment as well as tips to create a future-ready, efficient data center and ensure uptime.
By attending, you'll learn more about:
- Cost and energy savings associated with a completely contained data center rack
- The reasons for deploying airflow containment in facilities with power densities greater than 1 kW and up to 30 kW
- Cabinet design principles that provide optimal support and facilitate effective airflow
- Considerations needed for future designs of new or retrofitted data centers in order to get a substantial return on investment
You'll also find out how other businesses like yours have implemented the different types of airflow containment and are realizing the cost benefits today.
Register today. Can't attend, register anyway and we'll follow up with access to the on-demand webinar.
Posted by Brittany Mangan, Digital Content Specialist at 2/27/2020 11:11:30 AM