Cross-Connect Blog

New Chassis Design of CPI’s Evolution® Horizontal Cable Manager Addresses Airflow Management Best Practices

March 31, 2017

Evolution Horizontal Manager Chatsworth Products (CPI) has redesigned its Evolution® Horizontal Cable Manager to include a flared edge feature at the top and bottom of the manager, so that the entire rack-mount unit (U) space can be properly covered for optimal airflow management at the rack level.

Additionally, customers can now choose between solid chassis or chassis with cable openings. The solid chassis is recommended in applications where thermal isolation is important, such as in the front of rails of cabinets, or when Passive Cooling® is being deployed.

Evolution Cable Management is used in high-density cabling applications on open two- and four-post CPI Rack Systems, delivering increased performance to match the demands of today’s data center applications.

For more information on Evolution Horizontal Cable Managers, visit the product page.

Raissa Carey, Technical Writer

Search CPI in the News