CPI Announces In-Region Manufacturing of ZetaFrame Cabinet System in Asia-Pacific
May 04, 2023
We’re so excited about our expansion into in-region, Asia-Pacific-based (APAC) manufacturing of the award-winning ZetaFrame™ Cabinet System. We’re committed to expanding our its global manufacturing footprint and to serving our customers and partners in the APAC region.
Reintroducing the ZetaFrame™ Cabinet System
ZetaFrame Cabinet System is a highly engineered data center cabinet solution that delivers quick-turn, built-to-order configurability and industry-leading strength and dynamic load ratings for today’s most demanding, high-density compute and networking needs. It maintains the same physical footprint as existing CPI cabinets offered in the APAC region.

The ZetaFrame Cabinet System’s features puts it in a league of its own. Some of those include:
-
Fast Selection and Customization – A wide range of standard configurations and complimentary consultation services allow customers to create a tailored solution that meets their exact requirements.
-
Industry-Leading Load Capacity – A roll-formed, tubular and fully-welded steel frame architecture supports market-leading 2268 kg static and 1814 kg dynamic loads.
-
Integrated Cable and Airflow Management – Seamless integration with optional cable and airflow management accessories under a single part number ensures quick deployment.
-
Integrated Bonding – Doors and panels bond to the frame through the cabinet’s hinges and contact points, eliminating the need for attaching separate grounding straps to cabinet components.
-
Enhanced Cable Management – ZetaFrame’s simple and versatile cable management accessories can be used independently or in combination to accommodate a wide variety of applications.
With in-region manufacturing capabilities in China, CPI is taking an important, next step forward in growing the company’s global manufacturing footprint in another high-growth region. Read more about this exciting change in our press release here.
Posted by Angelique Pollock, Digital Content Specialist at 5/4/2023 1:29:31 PM