CPI to Demonstrate Liquid Cooling Capability at Data Center World 2023

May 08, 2023

At this week's annual AFCOM Data Center World conference and exhibition in Austin, TX (just a short drive south of CPI's Central TX facilities in Georgetown and Round Rock), Chatsworth Products will not only exhibit a full array of data center infrastructure solutions for customers and partners in booth 805, we'll be showcasing the company’s flagship data center cabinet solution, the ZetaFrame™ Cabinet System, specially outfitted with a dielectric liquid cooling solution from ZutaCore®, whose HyperCool® solution uses a two-phase, waterless, direct-on-chip method of removing heat away from the processors.

This innovative proof-of-concept hardware demonstration comes at a time when emerging technologies such as artificial intelligence and high-performance computing are driving increased need for more energy efficient methods of cooling and power consumption. Across the data center industry, such advancements are poised to help usher in a more sustainable, environmentally-friendly and carbon neutral technology infrastructure.
 
The hardware integration, made possible by ZetaFrame’s industry-leading 4,000 lb. dynamic load rating for an interior payload, supports a fully integrated rack containing ZutaCore components and enables secure transport of a loaded rack and cooling system when used in conjunction with a shock pallet. These components include the ZutaCore HyperCool manifold that easily mounts to CPI’s dual vertical power distribution unit (PDU) bracket using button mount features and a heavy-duty shelf support with transportation tie-down brackets for the ZutaCore HyperCool heat rejection unit (HRU). The unique setup also allows for easy integration of CPI’s popular, eConnect® Power Distribution Units (PDUs), standard ZetaFrame cable management and airflow management accessories.

Simply put, you're going to want to see this - and if you aren't attending the show, make a plan to follow CPI on social media for real-time updates and photos/videos from the booth, and this exciting new technology demonstration!

To learn about a few other highlights and surprises happening at this week's Data Center World, be sure to read the full press release.
Posted by Angelique Pollock, Digital Content Specialist at 5/8/2023 5:18:58 AM
Search CPI in the News