Forged by a
true pioneer spirit, the State of Montana inhabits a place (and
time zone) all its own - a place known simply as "Big Sky Country."
Yet for all its wide open spaces and natural wonder, Montana's true
grit resides in a rich tradition of capitalizing on "golden"
opportunities. Case in point? In a city where more millionaires
lived (per capita) than any other in the world at the turn of the
20th century, Helena, Montana is now home to a whole new kind of
goldmine - that of the first-ever United States data center to use
the remarkably efficient, energy recovery wheel, air-to-air heat
exchange cooling system known as KyotoCooling® - supported by CPI Passive Cooling®
Solutions.
But just how did the State of Montana go from a data center
operating at a frigid 45 degrees Fahrenheit just to cool blade
servers to a brand new facility reporting PUEs of an
astounding 1.08? Let's find out.
In 2007, the Montana State legislature appropriated funds for
two new data centers. With top-level goals in mind (reliability,
security, and efficiency) and a challenge from the governor - the
'20 by 10' initiative calling for energy
consumption in state-owned buildings to decrease by 20 percent
before the end of 2010 - two groups within the state's department
of administration set out on the job - Information Technology
Services Division (ITSD) and the Architecture and Engineering
Division (A&E).
Because of Montana's unique geographical location, weather
patterns and scarce population, the need for a reliable data center
was paramount - especially considering the state's citizens,
taxpayers and employees depend on the facility to manage everything
from payroll to medical info. Likewise, it was imperative to seek
solutions that would not only ensure reliability full stop, but do
so in a highly cost-conscious and environmentally-friendly
manner.
With all
planning pieces in place, the state then set its sterling
reputation for self-reliance to task, took a lead-by-example
approach, and set an innovative new precedent by selecting the
KyotoCooling thermal management technique, supported by Chatsworth
Products, Inc. (CPI) infrastructure storage and CPI Passive
Cooling®.
Thanks to plenty of prior analysis and research, the State of
Montana paired its thermal solution with CPI's F-Series TeraFrame®
Cabinets, equipped with Vertical Exhaust Ducts to allow
hot air to be directed out of the cabinets and into an isolated
return path above the drop ceiling. In isolating the hot return
air, it's then circulated and absorbed by the innovative Kyoto
wheel, and mixed with the seasonally cool, outside air to negate
the need for more traditional (and more expensive) methods of
cooling.
To truly appreciate what the State of Montana has accomplished
with this data center, CPI is teaming up with KyotoCooling and
industry experts to bring you the first-ever U.S.
KyotoCooling Conference - October 25-26, 2011. This is
your chance to tour the data center, meet the team, engage in
presentations by CPI's Ian Seaton, the Uptime Institute's Robert
"Dr. Bob" Sullivan, and the architect of KyotoCooling himself, Mees
Lodder. The best part of all? The conference is complimentary! Jeff
Cihocki, eContent Specialist