El siguiente software es compatible con una variedad de productos eléctricos y electrónicos de CPI. Seleccione el enlace de software apropiado a continuación. Para obtener ayuda, comuníquese con nuestro equipo de soporte técnico.
 

eConnect® Power Distribution Unit (PDU)

Un Archivo  Fecha de Lanzamiento Notas
Firmware 5.3.1054 07-07-2023 Use only with individual eConnect units with eConnect® Controller 4 (MCM4). This firmware revision is intended for individual eConnect PDUs with an eConnect Controller 4 (MCM4) and can be used in a Secure Array with eConnects that have eConnect Controller 3 (MCM3 controller) or eConnect Controller 2 (MCM2 controller) after those controllers are updated to firmware revision 4.11.731 or later. PDUs with this firmware revision cannot be used in Secure Array with PDUs that have an eConnect Controller 1 (MCM1 controller). 

Lea las Notas de la versión para más detalles (inglés)
 
Firmware 4.13.1054 07-07-2023 Use only with individual eConnect units with MCM3 or MCM2 controller; or if all units within Secure Array® have MCM3 or MCM2 controllers.This firmware revision is intended for individual eConnect PDUs with an eConnect Controller 3 (MCM3 controller) or eConnect Controller 2 (MCM2 controller) or eConnect PDUs within a Secure Array®, all of which have an MCM3 or MCM2 controller. Do not use this firmware version, if any of the PDUs within the Secure Array have an eConnect Controller 1 (MCM1 controller). 

Lea las Notas de la versión para más detalles (inglés).
 
Zero Touch Provisioning User Guide 07-29-2020 Use only with eConnect units with eConnect Controller 4 (MCM4) and firmware revision 5.2.757 or later. 
Command Line Interface User Guide 07-07-2023 Use only with eConnect units with eConnect Controller 4 (MCM4); or with eConnect units with eConnect Controller 3 (MCM3) and firmware revision 4.12.757 or later. Requires a serial console cord to connect a computer to the PDU. See guide for recommendations. Order the serial console cord separately.
RESTful API User Guide 07-07-2023  
SNMP MIB File 09-26-2022  
 

Networked RFID Electronic Lock Kit

Un Archivo  Fecha de Lanzamiento Manual / Notas
Firmware 5.3.1054 07-07-2023 Lea las Notas de la versión para más detalles (inglés)
Command Line Interface User Guide 07-07-2023 Use only with Networked RFID Electronic Lock Kits and eConnect units with eConnect Controller 4 (MCM4). Requires a serial console cord to connect a computer to the Networked RFID Electronic Lock Kit. See guide for recommendations. Order the serial console cord separately.
SNMP MIB File 07-07-2023  

Networked Electronic Access Control (EAC)

Un Archivo  Fecha de Lanzamiento Manual / Notas
Firmware 4.13.950 07-07-2023 Lea las Notas de la versión para más detalles (inglés).
Command Line Interface User Guide 07-07-2023 Use only with Networked Electronic Access Control (EAC) Kits or eConnect units with eConnect Controller 3 (MCM3) and firmware revision 4.12.757 or later. Requires a serial console cord to connect a computer to the Networked Electronic Access Control (EAC) Kit. See guide for recommendations. Order the serial console cord separately.
SNMP MIB File 07-07-2023  
 

Additional Power Distribution Units

Un Archivo  Fecha de Lanzamiento Usado con Estos Productos
MIB Files
1-21-2013
P/N 356XX- and 358XX-series Monitored and Controlled PDUs
Serial Access Program* 10-25-2010 P/N 356XX- and 358XX-series Monitored and Controlled PDUs 
 

IP KVMs 

Un Archivo  Fecha de Lanzamiento Usado con Estos Productos
Console Setup Software
11-11-2011
IP KVM Switch with Cat 5/6 Ports
IP KVM Switch with DB15 Ports
 

Remote Infrastructure Management (RIM) 

Un Archivo   Fecha de Lanzamiento Usado con Estos Productos
RIM-1000 Firmware **
7-14-2014
RIM-1000 
RIM-1000 MIB 7-14-2014 RIM-1000 
RIM-750 Firmware   RIM-750
Protocol Converter Firmware 7-14-2014 RIM Protocol Converter
Protocol Converter MIB 7-14-2014 RIM Protocol Converter

*El software en serie le permite acceder, configurar, monitorear y controlar las PDU seleccionadas mediante una conexión en serie directa a una computadora. Use el cable de configuración serial RJ-45 a DB-9 (P / N 35941-131) para conectar la PDU y la computadora. Tenga en cuenta que las PDU fabricadas después del 1 de septiembre de 2009 se pueden configurar utilizando un navegador web habilitado para Java en lugar de la configuración en serie.

**Póngase en contacto con el Soporte técnico al 800-834-4969 antes de instalar el firmware RIM-1000.