Cross-Connect Blog

Webinar: Build an Aisle Containment Solution without Replacing Cabinets

December 05, 2014

CPI Aisle ContainmentResearch suggests that most data centers use an average of four times the power for cooling than the IT load requires. With power requirements only going up; by some estimates, 30 to 50 percent of data centers will run out of power and cooling within the next year. 

Learn how to make the most of the power already being supplied to your data center with solutions that optimize airflow, reduce operating costs and eliminate the need to purchase additional CRAC units. 

Don’t miss this eye-opening webinar on power and cooling on Dec. 18 at 10:30 am Central Standard Time.

Chatsworth Products’ (CPI), Field Application Engineer, Tom Cabral, will delve into topics such as:

  • Benefits of isolation
  • Highlights of CA Title 24
  • The case for containment
  • Methods of containment…is one better than another?
  • Hot Aisle vs. Cold Aisle
  • A detailed study of containing an active data center

Register today.

Raissa Carey, eContent Specialist

Search CPI in the News
Get Blog Updates
Stay up to date on latest news and solutions.