Cross-Connect Blog

Seven Best Practices for Achieving Data Center Optimization

January 23, 2017

TeraFrame CabinetsWith technologies surrounding cloud computing and convergence evolving, data center managers should reshape their strategies to allow for greater capacity and ensure they can provide the highest quality of uninterrupted service.

Moreover, data center managers should work to identify where their resources are currently allocated and how they can best be optimized. The key to this is embracing the latest thermal efficiency, airflow and power and environmental monitoring strategies. The way data centers utilize their resources will undoubtedly continue to change as new technologies emerge. Furthermore, as more devices become integrated with the Internet of Things (IoT), downtime will not be an option.

Chatsworth Products (CPI) Product Manager, Luca Rozzoni, recently wrote an article on seven best practices for addressing these demands and achieving data center optimization:

  1. Address airflow management – The most critical step is separation of hot and cold air within the server room. There are three basic solutions: cabinet with Vertical Exhaust Duct, hot aisle containment and cold aisle containment.
  2. Remove barriers to increase power/heat densities – Isolation can be achieved by using accessories such as blanking filler panels, air dams and brush seal grommets
  3. Track rack conditions and environmental variables – It is important to work with solutions that can provide the ability to look into the thermal and environment performance of the infrastructure.
  4. Monitor power – Intelligent power distribution units (PDUs) with monitoring capabilities enable the monitoring of voltage, current, power (kW) and energy (kilowatt-hour) levels.
  5. Monitor cooling – Track inlet temperatures against the latest ASHRAE guidelines and evolving equipment specifications.
  6. Monitor uptime and status reports  Check individual system uptime reports and keep an eye on the status of various system regularly.
  7. Budget for new airflow and HVAC optimization systems – With a ducted exhaust system, every bit of cold air produced by the HVAC system has to go through a server, so there is no waste.

Enforcing these best practices and adopting the latest technologies will be vital in achieving a data center capable of supporting the needs of future technology demands.

Read Rozzoni’s article “Ready to Reshape” for more detailed information about achieving data center optimization. 

To learn more about how CPI’s data center infrastructure solutions support these best practices, visit our Energy Efficiency web page

Shannon Erdley, Public Relations Specialist

Search CPI in the News
Get Blog Updates
Stay up to date on latest news and solutions.