Cross-Connect Blog

New CPI Vertical Cable Manager Size Addresses Growing Cable Needs

November 17, 2014

Cable_Ring_for_GVCS.jpgYou can now support and organize larger bundles of high-performance cables with the newly available 10-inch wide Global Vertical Cabling Section (GVCS) and cable rings.

High-performance cables such as Category 6A, for example, are heavier and larger in diameter than their counterparts, so cable managers that will house these cables should be large enough to accommodate them.

The GVCS is an adaptable vertical cable management solution with a unique, two-piece design that reduces shipping size and cost.

CPI’s Cable Rings create a separate cable path on back of the GVCS to organize cables for a neat, professional installation. The rings can be added to the back of the single-side managers to create a front and rear pathway for cables.

For more information on the GVCS and Cable Rings, download the cut sheet.
  
Raissa Carey, eContent Specialist 
Search CPI in the News
Get Blog Updates
Stay up to date on latest news and solutions.