For most data center operators, aisle containment isn’t new. You probably added doors, roofs, or partitions and checked the “containment” box years ago.
But in practice, performance often falls short of the design promise. Small oversights can quietly drain cooling capacity, drive up fan energy costs, and limit your ability to scale high-density workloads.
If your PUE improvements have stalled, your fan speeds run higher than expected, or you’re planning to add liquid cooling, these persistent myths could be the hidden reason your airflow strategy isn’t reaching its full potential.
Myth #1: Containment Is Just About the Aisle
Most operators know to separate hot and cold zones, control mixing, and protect supply temperatures. But an aisle barrier alone is only as strong as its weakest link — and that weak link is usually inside the cabinet.
If airflow inside the cabinet is not controlled, aisle containment solutions will only be able to do half of the job. True containment means creating a continuous, sealed airflow path: from the supply plenum or perforated tile, through the cabinet, across the IT load, and into the return path — without shortcuts or leaks.
Think of it this way: aisle containment without cabinet-level control is like patching holes in a bucket but leaving the bottom open. You’re still paying to move air that never cools your servers.
Any low-resistance escape — an open U space, an unsealed cable cutout, a missing side panel — lets conditioned air leak out before it reaches your equipment. This can influence your predictable static pressure, weakens your cooling efficiency, and forces fans to work harder than they should.
Successful containment strategies recognize the cabinet as an active piece of your airflow system, not a passive frame. That’s why the most effective containment strategies address airflow at the cabinet, row, and aisle levels together.
Cabinet-level improvements that close the gaps include:
✔️ Installing to block unused rack units and force air through active gear.
✔️ Sealing cable openings with
✔️ Adding and to prevent air from escaping between cabinets.
Although these improvements may seem like small tweaks, they have direct impact on ROI. These low-cost fixes can deliver immediate, measurable gains — making sure your aisle containment works as promised, not just on paper.
Myth #2: “Retrofitting Containment Is Too Disruptive or Expensive”
It’s easy to see why this myth sticks around: many operators think if they didn’t design for containment from day one, they’re stuck with inefficient airflow — or that fixing it means tearing out rows, relocating live equipment, and absorbing downtime they can’t afford.
But the reality is, modern containment retrofits don’t look like they did 15 years ago. The industry knows most sites have legacy cabinets, overhead obstructions, or non-standard aisle dimensions. The best systems today are engineered to adapt around those constraints — with modular, scalable solutions that keep your environment online while you upgrade.
Where to start:
- Audit your highest-density rows to find the biggest thermal gaps.
- Pinpoint chronic hotspots or high recirculation zones that limit capacity.
- Use build-to-spec kits that adapt to your actual layout — not just an ideal design on paper.
How CPI’s solutions make retrofits practical:
Not every aisle is textbook — older environments often have uneven cabinet heights, irregular rows, or overhead barriers like cable trays and fire suppression pipes. CPI’s BTS Kits are modular and custom-fit to these real-world layouts. They provide a properly sealed containment system without costly construction or forced cabinet moves. The BTS Kit can be phased in row-by-row or aisle-by-aisle while keeping live systems running.
In high-density or mixed-density rows, vertical exhaust ducts are a proven retrofit tool. VEDs attach to the top of each cabinet, capturing hot exhaust air and channeling it straight back to the ceiling plenum — instead of relying on perfect aisle seals alone.
Because VEDs work with the physics of natural buoyancy and pressure differential, they often deliver immediate gains — especially when full aisle containment isn’t feasible due to building constraints.
Done right, retrofitting is one of the fastest, lowest-risk ways to reclaim stranded cooling capacity and prepare your environment for high-density workloads and future liquid cooling deployments.
Myth #3: Cabinet Design Doesn’t Matter If You Have Containment
Aisle and row containment work best when the cabinet is designed to do its part too — yet cabinet design is one of the most overlooked pieces of an effective airflow strategy.
A cabinet isn’t just a metal box to hold servers — it acts as a controlled plenum for directing conditioned supply air through your IT equipment and guiding exhaust air back to return.
When cabinet integrity is compromised, unintended low-resistance pathways that the air naturally prefers are created:
- An open rack unit (U space) means air leaks out before reaching hot IT loads.
- Unsealed cable openings become escape routes for conditioned air under positive pressure.
- Side vents or misaligned side panels let hot exhaust and cold supply air mix, undermining the aisle pressure differential you’ve built.
Successful cabinet design keeps airflow moving exactly where you want it: front-to-back through the equipment. Features like blanking panels, brush grommets, well-fitted side panels, and modular baffles seal off problem areas and maintain the static pressure your equipment needs.
What to check:
- Treat cabinets as adjustable airflow components — not passive frames.
- Choose cabinets with integrated sealing options: blanking panels, brush grommets, side fillers, and baffles.
- Validate side panel alignment and baying between cabinets.
- Reconfigure airflow seals as rack density and configurations change.
Cabinet design isn’t just about adding a few blanking panels after the fact. It’s about choosing, configuring, and maintaining cabinets that actively support your airflow plan.
Done right, your cabinets become a solid link in your containment strategy — not the weak point that quietly drains cooling capacity and adds to your fan energy bill.
Is Your Airflow Strategy Leaving Money on the Table?
Containment is not just an aisle-level fix. True efficiency requires a layered approach: cabinet, row, aisle — and the flexibility to adjust as your environment evolves.
CPI’s experts can help you identify where you’re losing efficiency—and how to fix it with a flexible, modular containment solution. Let’s make sure your aisle containment delivers the performance you expect.
.