As high-performance computing (HPC), artificial intelligence (AI), and machine learning (ML) workloads continue to drive up power densities in modern data centers, conventional air-cooling solutions are being pushed to their limits. To address these escalating demands, the University of Chicago independently validated the performance of an integrated waterless liquid cooling solution. Their findings deliver compelling evidence for the future of high-density, sustainable computing.
Through comprehensive side-by-side testing, the University compared waterless liquid cooling technology integrated into Chatsworth Products’ (CPI) ZetaFrame® Cabinet System against traditional rear door heat exchanger (RDHx) solutions.
The results reveal significant thermal and energy efficiency benefits, reduced internal cabinet temperatures, and consistent performance under demanding workloads.
The Challenge: Cooling at the Speed of Innovation
The University of Chicago’s research computing teams required a data center cooling solution that could meet the rapidly evolving, GPU-intensive workloads. With multiple research groups, including Maniac Lab, Toyota Technological Institute at Chicago (TTIC), and the Research Computing Center (RCC), relaying on dense compute clusters, effective thermal management was essential for growth.
Historically, the University’s utilized RDHx cooling, which operates by routing hot exhaust air to a rear-mounted coil for heat dissipation. While effective at lower densities, RDHx systems struggled to maintain safe internal temperatures as server power demands increased. The University sought a solution capable of directly and efficiently removing heat from within the cabinet, addressing the challenges of high-density environments head-on.
The Approach: Benchmarking Waterless Liquid Cooling Against RDHx
The University of Chicago independently deployed an integrated two-phase waterless liquid cooling solution featuring patented pool-boiling technology. This system dynamically adapts to varying heat generation, regardless of flow volume, ensuring optimal thermal management.
By utilizing cold plates placed directly on top of the processors, the University maintains consistent temperatures, effectively mitigating thermal shocks and enhancing silicon longevity, even during rapid power fluctuations common in AI workloads. This advanced cooling solution includes:
- from Chatsworth Products (CPI)
- for high-density power distribution
- , a direct-to-chip waterless liquid cooling solution
The proof of concept directly compared identical server hardware—with and without waterless liquid cooling—running the same workloads simultaneously. The test systems included Dell PowerEdge R6525 models equipped with AMD EPYC 7302 processors.
For seven days, the team rigorously tracked key performance indicators such as CPU temperatures, power consumption, noise levels, and compute performance.
The Results: Enhanced Cooling and Efficiency
The University’s independent testing revealed several significant advantages of the waterless liquid cooling system compared to RDHx:
- Substantially Lower Cabinet Temperatures: Average internal cabinet temperatures dropped from approximately 130°F with RDHx cooling to around 80°F with waterless direct-to-chip liquid cooling. This marked difference is achieved by directly transferring heat from CPUs into a specialized cooling loop, bypassing the inefficiencies of internal air heat buildup.
- 37% Reduction in Power Consumption: The waterless liquid cooled systems reduced energy by 37% compared to RDHx solutions, largely decreasing or eliminating the reliance on high-speed server fans.
- Sustained Performance Without Throttling: CPU temperatures remained within safe thresholds even under heavy computational loads, ensuring consistent performance for demanding HPC and AI tasks.
- Lower Fan Noise and Exhaust Heat: Noise and exhaust air temperatures were significantly reduced, making the system not only efficient but also more comfortable to operate.
These results validate waterless liquid cooling as a solution that supports high-performance environments while delivering energy savings and superior thermal management.
Lessons Learned and Next Steps
The success of the proof-of-concept generated excitement across the University of Chicago’s research teams. They not only recognized the operational benefits but also began planning for broader deployment of waterless, direct-to-chip liquid cooling across additional compute clusters.
Lessons learned from the deployment highlighted the importance of preparing for specific maintenance requirements, such as carefully managing temporary service interruptions and selecting robust, user friendly connection hardware.
Moving forward, the University intends to expand ZutaCore’s waterless liquid cooling cooling, fine-tune system configurations for job optimization, and explore further energy efficiency advancements.
Final Thoughts: Paving the Way for Sustainable HPC
The University of Chicago demonstrated the effectiveness of ZutaCore direct-to-chip waterless liquid cooling by integrating it with Chatsworth Products' ZetaFrame® cabinet system, achieving a 50°F reduction in cabinet temperatures and a 37% decrease in power consumption.
By cutting internal cabinet temperatures by over 50°F, reducing energy consumption by 37%, and maintaining consistent performance even under extreme workloads, the University’s has set a model for data centers striving to align with next-generation requirements.
This study underscores that the future of energy-efficient, sustainable, high-performance computing is already within reach.