Data center consolidation remains one of the most disruptive projects an operator can undertake. Done well, it can deliver efficiency gains, reduced overhead, and alignment with long-term IT and business strategies. But the reality is rarely straightforward.
At Chatsworth Products (CPI), we’ve spent more than three decades helping operators navigate these challenges. The perspective shared here draws on the expertise of Steve Bornfield, Senior Data Center Consultant at CPI, who has led numerous customers through complex consolidation and migration efforts as well as new build plans. His experience informs the risks, trade-offs, and practical considerations outlined below.
Steve’s focus is on solutions that are cost-effective, efficient, and sustainable—helping operators minimize downtime, reduce risk, and emerge with an environment that is leaner, more resilient, and built for future growth.
Risks and Realities of Consolidation
Consolidation isn’t just about reducing footprint—it’s about managing uncertainty, protecting uptime, and aligning the outcome with long-term business and sustainability goals.
Before beginning a data center migration or consolidation project, operators should acknowledge the common pitfalls:
- Unpredictable outcomes – Initial assessments often overturn assumptions about which facility is “worth keeping.” Portfolio decisions rarely follow the neat logic expected at the start.
- Hidden inefficiencies – Ghost servers, abandoned cabling, and stranded cooling or power capacity frequently surface mid-project. Without reliable visibility—typically provided by DCIM—these inefficiencies remain invisible until they disrupt timelines.
- Shifting priorities – ESG requirements and sustainability reporting increasingly influence decisions, with cost balanced against the carbon footprint of the retained site.
- Operational disruption –Even the best-laid plans introduce downtime risk. Consolidation succeeds when operators build in flexibility and treat migration as an iterative process rather than a single cutover.
Data Center Consolidation Checklist: Key Domains to Evaluate
1. Power & Redundancy
Published megawatt figures rarely tell the whole story. What matters is the true, usable power inside the facility—and whether the supporting infrastructure can sustain higher consolidated loads over time.
- Validate usable vs. stated capacity. Stranded circuits and cooling dependencies often reduce what’s actually available.
- Assess feed resilience and uptime history. Dual feeds on paper don’t guarantee past performance; review maintenance logs and outage records.
- Evaluate UPS condition and efficiency. Aging fleets, low-efficiency units, and limited replacement cycles can undermine consolidation ROI.
- Plan for future density. Confirm support for higher voltages (e.g., 240/415V) and the ability to accommodate rack densities beyond today’s averages.
- Use DCIM for visibility. A mature provides a single pane of glass across legacy and new environments, guiding both current capacity use and future build plans.
2. Cooling Infrastructure
Consolidation projects are where cooling limitations surface fastest. Merging workloads into fewer sites raises density, stresses legacy plants, and forces a decision: extend the life of existing systems, or use consolidation as the inflection point for liquid adoption.
- Treat consolidation as the trigger to realign cooling strategy. A short-term patch might save budget today but often locks you into stranded capital and another disruptive upgrade cycle within a few years.
- Audit efficiency and capacity headroom. Legacy DX and chilled water plants may look sufficient on paper but can mask stranded capacity that undermines consolidation ROI.
- Model future density curves. AI/HPC workloads can push racks to 30–60 kW or higher. If you’re consolidating enterprise workloads alongside AI, plan for blended density and phased transitions.
- Evaluate retrofit economics. Containment or rear-door heat exchangers may buy time but weigh their cost and disruption against moving directly to cabinet- or chip-level liquid cooling.
- Plan for transition risk. Consolidation magnifies the impact of downtime. Model how cooling upgrades—whether phased or wholesale—can be executed without destabilizing live environments.
3. Network Positioning and Power
In consolidation, connectivity matters—latency, route diversity, and peering define performance—but only after power capacity makes the site viable.
- Confirm utility capacity and expansion potential. Consolidation often pushes sites beyond their designed envelope; power is the gating factor.
- Map carriers, route diversity, and peering. Connectivity is critical for performance, but rarely the deal-breaker if power is constrained.
- Measure latency to cloud and interconnection hubs. Low-latency routes protect workload performance post-consolidation.
- Review contractual obligations. Utility agreements, carrier contracts, and cross-connect terms can all affect timing and cost.
4. IT Hardware & Workload Lifecycle
Hardware lifecycle isn’t just a technical detail—it’s often the lever that determines what consolidates first, and what can be retired altogether. End-of-life systems often create natural exit points, while supported platforms shape the balance between on-premises, colocation, and cloud.
- Inventory hardware with context. Age, support contracts, and licensing status determine not just replacement cost but also consolidation sequencing.
- Flag EOL workloads early. These are often the lowest-friction candidates for decommissioning and can reduce the consolidation footprint quickly.
- Map application placement. Distinguish which workloads justify staying on-prem (performance, compliance, latency) versus those better suited for cloud or colocation.
- Model licensing and support economics. Renewal cycles can be a hidden driver of consolidation timing.
5. Space & Layout Utilization
Cabinet-level accuracy is critical to prevent hidden inefficiencies. Without precise cabinet-level data, consolidation plans risk being built on false assumptions about available space and capacity.
- Update cabinet documentation. Device location, connectivity, and dependencies must be current; DCIM provides the needed visibility at this level.
- Expose stranded capacity. Stranded RU, weight, or airflow constraints distort usable space and must be corrected before consolidation math is reliable.
- Evaluate airflow and cabling against density goals. A site that looks spacious on paper may already be thermally or structurally maxed out.
- Enforce structured cabling and intelligent PDUs. Consolidation is the moment to eliminate legacy cabling sprawl and adopt power distribution that supports monitoring and control.
6. Compliance & Security
Consolidation projects carry heightened compliance and security risk. Moving workloads across sites can expose gaps in regulatory coverage or weaken physical security if controls aren’t uniformly enforced. Sustainability reporting is now also part of the equation, influencing both site selection and stakeholder approval.
- Verify regulatory readiness. Confirm frameworks such as HIPAA, PCI DSS, GDPR, or SOC 2 are consistently supported across target sites.
- Audit physical security and monitoring. Badge systems, cameras, and access logs must align to prevent weakest-link vulnerabilities during or after consolidation.
- Assess sustainability metrics. Energy efficiency, water use, and carbon intensity increasingly shape decisions—especially in investor- or customer-driven markets.
Get Expert Help from CPI
Successful consolidation depends on getting the fundamentals right—power, cooling, cabinets, and cable management. For over 30 years, Chatsworth Products (CPI) has provided the infrastructure and expertise to help operators reduce risk, improve efficiency, and prepare for future growth.
Ready to start planning? for a free consultation and see how we can help simplify your consolidation.