AI and high-performance computing (HPC) are here, and they’re driving rack densities to 30, 45, even 60 kW and beyond. But while compute accelerates, legacy infrastructure is lagging. For data centers originally designed for 5 to 10 kW per rack, airflow, power distribution, and cabinet design are now becoming constraints.
Scaling to high density isn’t just about adding more capacity or even chasing the newest technology—it’s about managing greater complexity with smarter, more resilient core infrastructure choices.
Below, we examine five core areas where high-density is redefining requirements—and what operators need to do to keep pace.
1. Airflow Management: The First and Often Overlooked Bottleneck
Liquid cooling is advancing fast. But for most data centers, air cooling is still doing the heavy lifting—especially in hybrid environments. Even in hybrid cooling environments, where liquid removes part of the load, residual air cooling is essential.
The challenge is simple: more heat in less space leaves less room for error. Even small lapses in airflow control—unsealed cable cutouts, gaps between cabinets, mismatched row configurations—can lead to recirculation, hot spots, and overworked cooling systems.
At Chatsworth Products (CPI), we’ve seen it firsthand across hundreds of deployments: basic airflow missteps quietly draining efficiency and driving up thermal risk.
The opportunity is clear: airflow containment is one of the fastest, most cost-effective ways to regain control. When properly implemented, it improves reliability, reduces energy use, and often postpones the need for capital upgrades.
"We found that CPI’s containment strategies reduced our energy usage by 25–30%, simply by improving airflow control. It allowed us to postpone a major chiller upgrade."
Eric PattersonCDW Corporation
Field-Tested Approaches to Optimize Airflow:
- Cabinet-Level Solutions: As rack densities increase, you need airtight airflow control right at the source. That’s where CPI’s cabinet-level thermal management accessories and comes in—removing heat directly from the rack before it disrupts the surrounding environment.
- Tool-Less Retrofits: Need better airflow containment but can’t afford a major retrofit? offers a fast, low-disruption upgrade. Designed for hot aisle and row-based vertical exhaust duct configurations, it features telescoping panels and preassembled frames for quick installation.
- Build-to-Spec Containment: For more complex environments—like rooms with different cabinet sizes or unusual layouts— provides a customizable, field-assembled containment solution. It ensures a tight seal for either hot or cold aisles, maintaining thermal separation and efficiency across nonstandard setups.
- Computational Fluid Dynamics (CFD) Modeling: Not sure where the airflow issues are? CPI offers complimentary to pinpoint airflow inefficiencies, identify thermal hotspots, and guide targeted, high-impact improvements.
Whether liquid is part of your plan now or later, optimized airflow is the foundation every high-density deployment depends on.
2. Rethinking Power for High-Density Compute
Rack consolidation has fundamentally reshaped the rules of power infrastructure. Where 20 racks once distributed load, three now carry it—each pushing up to 60 kW in environments reaching 149°F (65°C). Legacy PDUs weren’t built for this level of heat, density, or operational risk.
This isn’t just about delivering more power—it’s about supporting dramatically more compute in far less space. As
“In practice, this means reducing from 24 racks in an early HAC design to as few as three high-power racks in the future—without expanding the data center’s footprint.”
NVIDIA’s Wade VinsonData Center World 2025
Fewer racks doing exponentially more work means power delivery must scale, stabilize, and self-monitor—without compromise.
In high-density environments, data center performance hinges not just on how much power you can deliver—but how precisely and efficiently you can manage it.
That’s why modern PDUs must deliver:
- High power configurations (typically 20 kW–60 kW or more per unit)
- Reliable operation at high temperatures (e.g., rated for 149°F / 65°C ambient)
- Outlet-level metering and switching for real-time visibility and control
- Integrated branch circuit protection, to isolate and contain localized issues
- Accurate metering and load balancing, to optimize usage and reduce waste
- Compatibility with DCIM tools, for centralized oversight and data-driven automation
Chatsworth Products’ are engineered for this new reality—offering configurations up to 57.5 kW, full outlet-level intelligence, and thermal resilience up to 149°F (65°C). When integrated into CPI’s cabinets, they simplify deployment and give operators the control they need—at the point of highest risk.
As demands rise, only precision-built systems will keep performance, risk, and cost in balance.
3. Why Most Cabinets Can’t Handle What’s Coming
The cabinet is no longer just a frame for mounting equipment. In today’s AI and HPC environments, it’s a structural, thermal, and operational node—and, increasingly, a limiting factor.
Modern workloads are heavier, hotter, and more complex. Cabinets now support far more than IT gear: integrated power distribution, liquid cooling manifolds, sidecars, rear-door heat exchangers, and dense cabling all contribute to load. Enclosures must retain structural integrity through shipping, installation, and—in many cases—seismic conditions.
At the same time, cabinets are now part of the airflow and containment architecture. Cabinet designs that fail to accommodate vertical exhaust ducts, baffles, or ceiling plenum integration can undercut the efficiency of even the most advanced cooling strategy. Gaps, obstructions, or incompatible form factors quietly erode thermal efficiency and undermine otherwise sound cooling strategies.
Modularity and serviceability, once afterthoughts, are now essential. Cabinets that can’t adapt to evolving footprints or allow clean access for moves, adds, and changes (MACs) introduce operational drag—and risk. And as racks fill edge-to-edge with high-value gear, the cost of poor design escalates.
The from Chatsworth Products is built for this next chapter. It’s the only cabinet on the market that combines:
- Industry-Leading Strength: Supports up to 5,000 lb. static / 4,000 lb. dynamic load
- Integrated by Design: Ships with eConnect® PDUs, cable managers, sensors, airflow accessories, and optional liquid cooling—minimizing deployment time and integration risk
- Complete Customization: Configure to exact specs without long lead times—and adapt as your environment evolves
In short, the ZetaFrame Cabinet is a platform built to carry your infrastructure into the future.
4. Monitoring: Visibility Where It Matters
At 30, 45—even 60 kW per rack—the stakes rise sharply. Thermal and security issues don’t usually start at the room level. They start at the cabinet. And in high-density environments, small anomalies quickly escalate into real threats.
A slight rise in inlet temperature. A humidity shift in one vertical zone. A cabinet left unlocked. In high-density environments, those are no longer minor anomalies—they’re precursors to failure.
The model is shifting. Monitoring can’t be centralized anymore. It must be distributed—intelligent at the edge, proactive at the cabinet.
Environmental monitoring needs to be localized and layered: sensors at intake and exhaust, at multiple heights, and across front and rear zones. Hybrid cooling and partial containment introduce uneven airflow patterns—and that’s exactly where hotspots form. Without cabinet-level data, these deviations remain invisible until they’ve already impacted performance.
As liquid cooling becomes more prevalent, leak detection at the cabinet level is also critical. Rear-door heat exchangers, direct-to-chip cold plates, and manifolds bring fluid directly into the rack. Monitoring systems need to catch leaks at the source—before they spread downstream or trigger equipment shutdowns.
Security, too, now starts at the rack. In colocation, lights-out, or unmanned sites, electronic locks and real-time access logs aren’t just safeguards—they’re compliance requirements. Physical access must be monitored and controlled just as closely as power and cooling.
CPI’s are purpose-built for this new standard. With outlet-level power monitoring, integrated environmental sensors, and electronic access control—all in one system—they give operators cabinet-level visibility and control. Factory-installed in CPI cabinets, they streamline deployment and ensure everything works together from day one.
Real-time visibility isn’t just about awareness—it’s about avoiding costly mistakes before they happen. The closer you can monitor, the better you can manage—and the faster you can respond.
5. Cabling: Not Just a Clutter Problem
More power means more cords. More compute means more connections. And in high-density environments—especially those supporting rear-door heat exchangers, liquid cooling manifolds, or overhead containment— where every inch of space is in use — every obstruction matters.
What’s often overlooked is how cabling itself can compromise airflow. Dense bundles act as baffles, disrupting pressure zones, creating turbulence, and reducing the effectiveness of even well-designed containment systems.
As the Uptime Institute noted in its 2024 Global Data Center Survey, “Even subtle design decisions—like cabling pathways—can have measurable impact on rack thermal performance and operational risk.”
Beyond airflow, dense cabling takes a physical toll: added weight stresses mounting points, restricts access, and raises the risk of accidental disconnections during routine maintenance. Too many cable managers look adequate when empty—but under real-world loads, they deform, sag, or compromise serviceability.
Modern cable managers must do more than tidy things up. They must:
- Maintain separation between data and power to reduce interference and ensure signal integrity
- Preserve cold and hot air separation by eliminating cable blockages in airflow pathways
- Support predictable bend radius and strain relief to extend cable life and minimize transmission loss
- Enable clean access for rapid MACs (Moves, Adds, Changes) without disrupting adjacent equipment
And compatibility matters. Fiber, for example, requires more finesse. CPI’s Motive® Cable Manager is engineered specifically for high-density fiber environments—protecting bend radius and ensuring performance isn’t compromised.
CPI addresses this with a wide range of tool-less, high-capacity engineered for strength, airflow performance, and ease of use. Designed to install quickly and support intuitive servicing, these systems maintain order under load—so you can maintain uptime under pressure.
Because in high-density environments, cable management isn’t secondary —it’s critical infrastructure. And managing it right protects everything else.
Not sure where to start? Get expert help from CPI
Chatsworth Products is a trusted leader in data center infrastructure—delivering cabinet systems, power management, and airflow solutions engineered for today’s high-density environments.
Our experts can help you build smarter with:
- Free CFD analysis to uncover airflow inefficiencies
- Expert guidance on cabinet strategy for high-density compute
- Power and cable management recommendations tailored to your layout
with our data center experts and take the guesswork out of scaling your infrastructure.