Thermal performance isn’t just about advanced cooling systems — it’s about how effectively the small details work together. A well-sealed, well-monitored rack is the foundation of an energy-efficient data center, yet it’s often the simplest components — blanking panels, air dams, and seals — that are overlooked.
The irony? These small parts can have a bigger impact on efficiency (and your cooling bill) than major infrastructure upgrades. By eliminating bypass airflow, preventing recirculation, and sealing leaks, the right rack-level accessories ensure every kilowatt of cooling does useful work.
Below are the thermal management accessories that you shouldn't deploy without:
1. Blanking or Filler Panels: The Simplest Way to Stop Air Recirculation
Blanking panels or aren’t new or flashy — and that’s often exactly why they’re overlooked or installed inconsistently. Yet few components have such a direct influence on rack-level airflow.
When even a few rack units are left open, hot exhaust air from active equipment flows back through those gaps, mixing with the cold intake air. The result is higher inlet temperatures, thermal imbalance across the row, and increased fan speeds that drive up energy use.
In computational fluid dynamics (CFD) models, seemingly minor recirculation paths can raise local inlet temperatures by 5–10°C — enough to reduce equipment reliability or trigger unnecessary cooling responses.
Properly installed blanking panels (also called filler panels) create a continuous barrier that separates the cold and hot zones within the cabinet. This ensures air follows its intended path: cold air in through the front, hot air out through the rear.
Why it matters:
- Closes gaps that cause recirculation
- Keeps cold air directed through equipment intakes
- Stabilizes inlet temperatures and reduces localized hotspots
- Improves overall cooling efficiency without additional airflow
Even in well-contained environments, maintaining a fully sealed rack face is one of the simplest, lowest-cost ways to preserve thermal integrity — and one of the first steps toward lowering cooling energy at scale.
Filler Panels block unused rack spaces in the ZetaFrame® Cabinet to stop recirculation and improve cooling efficiency.
2. Air Dams: Directing Air Where It Matters Most
Even with blanking panels in place, small volumes of air can still escape around the sides, top, or bottom of mounted equipment. These bypass paths might seem insignificant, but when multiplied across multiple cabinets, they can represent a substantial loss of cooling efficiency. Air intended for the equipment face instead follows the path of least resistance, diverting through these gaps and bypassing server intakes altogether.
Air dams mitigate this by sealing the perimeter of the rack space, ensuring consistent pressure differentials across the cabinet and stabilize inlet temperatures, even as rack densities increase.
What you gain:
- Improved cooling efficiency without increasing airflow volume
- Uniform temperature distribution across rack-mounted equipment
- Greater predictability under dynamic IT loads
- Lower overall cooling energy and fan utilization
When airflow is properly contained, less conditioned air is needed to maintain target inlet temperatures. This not only reduces fan energy consumption but also minimizes temperature variations that can lead to hotspots or erratic thermal performance across the row.
3. Vertical Exhaust Ducts: Turning the Cabinet into a Containment System
Containment doesn’t have to begin at the room level — and, in many environments, it’s more effective when it starts at the rack. Vertical exhaust ducts, sometimes referred to as chimneys, convert an individual cabinet into a self-contained thermal system by channeling hot exhaust air directly into a ceiling plenum or return duct.
By physically separating exhaust air from the cold room environment, these ducts eliminate hot-aisle recirculation and stabilize inlet temperatures across the row. The result is a more predictable and efficient airflow pattern that allows operators to safely raise supply-air temperatures without compromising equipment reliability.
In practice, cabinet-level or row-level containment can reduce energy consumption by 20–40% compared to open hot-aisle configurations, depending on facility design. It also helps balance mixed-density deployments, where conventional airflow distribution often struggles to maintain uniform conditions.
Why it matters:
- Isolates and removes hot exhaust air at its source
- Prevents hot/cold air mixing and reduces bypass airflow
- Enables higher supply-air temperatures and lower cooling energy use
- Maintains consistent inlet conditions across varying rack densities
Cabinet-level or row-level containment provides a scalable, modular approach to airflow management — one that can be implemented incrementally without major facility modifications while still delivering measurable gains in cooling performance and efficiency.
CPI Vertical Exhaust Duct channels hot exhaust air from cabinet tops to the return plenum for effective containment.
4. Grommets and Brush Kits: Containing Every Cubic Inch of Airflow
Even in well-sealed cabinets, one of the most common—and least quantified—sources of thermal loss occurs where cables pass through structural openings. Every cutout along a mounting rail, cabinet top, or raised-floor tile is a potential escape route for conditioned air or an entry point for exhaust heat.
Flexible brush strips and sealed grommet inserts allow cables and power cords to pass through while maintaining a physical barrier that preserves pressure and directionality within the airflow path.
Several configurations are commonly used to control leakage across different parts of the rack:
- – Ideal for high cable density or frequent moves, adds, and changes. The flexible brush material lets you pass or reroute bundles easily while maintaining an effective air barrier. Commonly used in mounting rails and side panels.
- – Provide a tighter mechanical seal for situations where cables are more static or airflow containment is critical. Snap-on or cut-to-fit grommets are useful along wider equipment rails or cabinet sides where precise sealing is required.
- Side panels with or seals – Enable lateral cable routing between cabinets while keeping exhaust air contained.
- – Used to seal cable openings under raised floors, maintaining underfloor pressure and reducing bypass airflow. Dual-layer brush and membrane designs allow cables to pass through without capturing them, simplifying maintenance.
When applied consistently, each of these solutions helps reduce bypass airflow, stabilize cabinet pressure, and improve overall cooling efficiency—without altering mechanical systems or changing airflow volume.
Equipment rail brush kits, raised floor grommets, and side panels with brush sealed cable openings help maintain airflow integrity.
5. Environmental Sensors: Quantifying the Effect
Airflow management improves predictability, but without data, it’s difficult to confirm how effective those changes truly are. positioned within key airflow paths provide the visibility needed to validate improvements, fine-tune cooling set points, and maintain stable conditions over time.
These sensors create a feedback loop between infrastructure and environment, allowing operators to measure performance instead of assuming it. The resulting data supports more precise control directly affecting energy consumption and equipment reliability.
Why it matters:
- Detects localized temperature anomalies before they escalate
- Enables proactive adjustments to fan speeds and cooling output
- Provides empirical data to justify higher supply-air temperatures
- Supports ongoing optimization and long-term thermal stability
By continuously monitoring conditions at the rack level, data center teams can transition from reactive cooling management to a more data-driven approach—one that maintains efficiency under changing loads and validates that airflow strategies are delivering measurable results.
Integrate Smarter Cooling Accessories into Your Next Cabinet Deployment
The most effective thermal strategies are designed in—not added later. At Chatsworth Products (CPI), we engineer the physical infrastructure that keeps critical IT equipment performing reliably, helping organizations operate efficiently as densities and thermal loads increase.
With our ZetaFrame® Cabinet System, thermal management accessories can be factory-installed to form a cohesive, rack-level ecosystem that delivers measurable gains from day one.
- with integrated thermal management accessories
- Explore our broad portfolio of