For all the focus on high-density compute and advanced cooling, one fundamental constraint is still catching many operators off guard: power readiness at the cabinet level.
As AI and HPC workloads grow more power-hungry and thermally demanding, the limits of legacy power assumptions — from breaker sizing and voltage to outlet capacity and form factor — are becoming impossible to ignore. Facilities that appear power-ready on paper can still hit deployment delays, stranded capacity, or costly rework when that power must be delivered reliably and efficiently inside the rack.
Avoiding this next bottleneck means rethinking how power architecture scales in practice — all the way from the upstream feed down to the cabinet floor.
Design vs. Reality: Why AI Rollouts Stall at the Rack
AI requires a new power strategy, not just more power. For years, many operators have treated power planning as a facility-wide question — focusing on total megawatts available, upstream distribution, and room-level redundancy. But modern AI workloads reveal a sharper reality: power readiness must extend all the way to the rack. This is where theoretical capacity collides with physical limits — breaker ratings, outlet density, cord routing, connector fit, and airflow clearance.
Several technical realities bring this into focus:
- Rising per-device draw: A single AI GPU power supply can draw 3kW or more of power, driving individual server loads to 20kW or higher and rack loads to 40kW and higher— a level that strains legacy assumptions about voltage and current.
- Non-uniform loading: N+1 or N+2 internal redundancy schemes common in GPU nodes create asymmetric loads that the classic A/B feed design was never built to handle effectively.
- Competing real estate: Liquid cooling hardware, bulkier heatsinks, and rear-door heat exchangers now compete for the same physical space as power units and cabling, further tightening the margin for error.
In short, a facility’s total power capacity may look sufficient on paper — but it’s the cabinet where bottlenecks occur, inefficiencies build up, and capacity can be stranded. For operators rolling out dense, GPU-based workloads at scale, treating cabinet-level power design as a secondary detail is increasingly untenable.
Five Power Pitfalls to Avoid in AI Rollouts
1. Defaulting to 208V
Many U.S. deployments default to 208V, unaware of the limitations it imposes at scale. 208V systems require higher current to deliver the same power as 240/415V, leading to inefficiencies, voltage drop, and limited scalability. Higher voltage three-phase systems reduce current draw, enabling denser power delivery with smaller conductors and less heat generation.
In the U.S., many operators stick with 208V because it’s familiar. But delivering higher total power at a lower voltage means higher current—requiring larger conductors, bigger breakers, and increasing voltage drop across distances.
A better approach is to design for 240/415V three-phase power:
- You reduce current draw for the same kW load.
- You lower conductor size requirements, saving copper costs and space.
- You cut down on resistive losses and waste heat.
For example, a rack delivering ~17 kW at 208V three-phase may require a 60A amps feed. At 240/415V, the same load requires a 32A feed—a nearly 50% reduction in current.
2. Undersized Breaker Capacity
Many legacy deployments still rely on 20A branch circuits on Rack power distribution units. Yet many modern GPU nodes draw 10–13A per PSU at 208V. 20A rated breakers with a maximum regulatory allowed continuous draw of 16A does not allow for optimal utilization of breaker capacity.
Shifting to 30A breakers—supported by compatible PDUs—reduces the total number of branch circuits required, easing installation and improving cabling efficiency. 30A breakers also allow for better use of breaker capacity while providing more margin for growth.
3. Misaligned Redundancy Models
In the enterprise world, the classic “dual power supply = A/B feeds” model assumes each supply draws 50% load. But AI servers commonly use N+1 or N+2 Redundancy for their performance requirements that puts significantly higher strain on the current draw for each branch circuit.
Intelligent PDUs with outlet level metering allow thresholds and notifications to be set at the branch circuit and outlet level allowing operators to manage power effectively and respond to impending issues.
4. Underestimating Outlet Layout
High-density servers typically include multiple power supplies per node, each drawing significant current. When total rack loads climb, it’s not uncommon to find dozens of power connections per cabinet.
If the deployed PDUs do not use Balanced Phase Outlets, operators often add more outlets to spread the load safely. But this approach introduces additional challenges:
- More outlets mean more power cords, increasing cable congestion that can obstruct critical airflow pathways.
- Excess cables complicate bend radius management, making it harder to maintain clean, efficient routing in tight rack spaces.
- A higher outlet count without intelligent monitoring reduces visibility into which connections are carrying load—and by how much.
A better practice is to specify PDUs with Balanced Phase Outlets that allows use of shorter power cords, simplifying installation and troubleshooting with minimal obstruction to airflow.
CPI's eConnect® PDUs come with QuadLock Outlets that provide flexibility of equipment that can be connected while ensuring that no inadvertent dropped loads happen due to loose cords.
5. Overlooking Form Factor and Integration Pain
Many off-the-shelf PDUs remain 3–4 inches wide. In dense AI cabinets, this footprint can obstruct airflow or interfere with liquid cooling manifolds.
In addition, high-power PDUs are physically heavier and more complex to install, increasing labor time and the risk of suboptimal cable routing.
A best-practice approach includes:
- Specifying PDUs with a slim profile (around 2.2 inches) to maximize airflow pathways.
- Planning for factory pre-installation of PDUs and cables to reduce onsite handling, installation risk, and time-to-operation.
How eConnect PDUs Deliver AI-Ready Power at Scale
Chatsworth Products’ are engineered specifically to eliminate the bottlenecks that stall high-density rollouts, so you can scale compute with confidence.
- More than 100 standard high-power PDU configurations, with lead times as short as 15 days
- Full support for 240/415V three-phase systems and 30A circuit breakers to deliver maximum capacity with less cable congestion
- A slim 2.2" form factor that preserves airflow pathways and integrates cleanly alongside liquid cooling hardware
- Switched and metered models for granular outlet-level monitoring, load balancing, and remote control
- Optional factory pre-installation in ZetaFrame® cabinets to reduce installation time and risk
- QuadLock Outlets support C13, C15, C19, and C21 outlet types with a built-in locking mechanism—no proprietary cords needed.
Explore the full range of today.