When you’re planning a deployment or maintaining a high-density rack, the last thing you want is to be held up by power issues at the outlet level. But that’s exactly what happens in many data centers. A plug doesn’t fit. A cord slips out. A PDU can’t handle the load.
These problems may seem minor at first, but they can quickly lead to delays, unplanned outages, and added complexity—especially when time, space, and reliability are already under pressure.
In demanding environments like edge deployments or AI-intensive workloads, reliability begins with smart outlet design. In this post, we’ll break down four often overlooked yet critical PDU outlet features that can help you avoid these pitfalls and deliver dependable power where it matters most.
How to Support Multiple Plug Types in a Rack—Without Adapters or Extra PDUs
If you're managing IT racks, you’ve probably hit this snag: A new device arrives. You go to plug it in—and it doesn’t fit your PDU.
This scenario is all too common in modern data centers, especially in high-density racks with a mix of hardware. You’ve got different generations of equipment, from different vendors, with mixed plug types in the same rack, outlet compatibility can become a real deployment obstacle.
And yet, most PDUs only support one or two outlet types. That means you're left dealing with:
- Devices not fitting your PDU, causing last-minute delays
- Adding adapters that eat up space, generate heat, and create more points of failure
- Buying extra PDUs just to support different plugs
- Reworking your layout, which adds time and increases the risk of downtime
The good news? There are newer PDUs designed to avoid all of this.
One option to consider is , which supports four outlet types – C13, C15, C19, and C21 – within a single unit, featuring an integrated locking mechanism and eliminating the need for adapters or additional equipment. They give you the flexibility to power a wide range of devices while keeping things simple and organized. And since they include built-in locking mechanisms that don’t require proprietary power cords, cords stay secure without the need for special accessories.
Increase PDU Capacity Without Adding More Units
Adding more powerful equipment shouldn't mean reworking your entire rack layout—but for many data center teams, that’s exactly what happens. AI and GPU-based workloads are pushing energy demands beyond what traditional PDUs can handle. And in high-density environments, that creates a real problem.
To compensate, teams often add more PDUs per cabinet—but that creates its own challenges: more cabling, more heat, more airflow restrictions, and more equipment to manage.
Choosing a high-power PDU instead allows you to deliver more energy per unit, which can:
- Reduce the number of PDUs per rack
- Streamline cable management
- Improve cooling efficiency and airflow by reducing cable congestion and creating space for advanced thermal strategies like liquid cooling
- Support high-performance compute without added infrastructure
Not all high-power PDUs are the same. As you evaluate options, consider:
- Input capacity – Can the PDU support 208V or 415V power with up to 100A inputs?
- Outlet density and configuration – Will it deliver enough outlets to support your mix of equipment?
- Monitoring and redundancy – Do you need visibility at the outlet level? Redundant power feeds?
- Compatibility with cabinet layout – Will it fit within your existing infrastructure without major redesigns?
CPI’s are one of the best high-power PDUs for data centers with a wide range of options built specifically for these demands, including models that support up to 100A inputs, 30-amp circuit breakers, and power capacities up to 57.5 kW per cabinet.
Keep Power Cords Secure Without Extra Hardware
Power cords disconnecting unexpectedly is one of the most frustrating and preventable issues in a rack environment. In high-density deployments—especially those supporting edge, AI, or GPU-heavy workloads—tight spaces, vibrations, and airflow pressure can cause cords to work themselves loose over time.
To reduce the risk, many data center teams turn to:
- External locking clips or cord retention brackets
- Specialty locking power cables
- Manual routing workarounds during install
But these solutions come with their own drawbacks—they add installation complexity, require proprietary parts, and increase the chance of human error during setup or maintenance.
Instead of adding hardware, a better way to prevent accidental disconnection of server power cords is to use PDUs with integrated outlet-level locking—a design that holds cords firmly in place without requiring proprietary power cords, special cables, or external accessories.
If you're looking for a reliable way to keep power cords secure in high-traffic or high-vibration environments, integrated locking outlets are an easy way to keep cords secure and avoid downtime.
Speed Up Installs and Troubleshooting with Color-Coded Outlets
When you're under pressure to restore service or make changes fast, digging through a tangle of identical cords can waste valuable time—and lead to costly mistakes.
That’s why more data center teams are turning to PDUs with color-coded outlets. It's a simple visual aid that can make a big difference when it comes to:
- Quickly identifying which outlet is tied to which circuit or breaker
- Balancing loads across phases more effectively
- Reducing human error during installs and maintenance
- Speeding up moves, adds, and changes with less guesswork
Color-coding is more than a convenience—it’s a visibility tool that directly improves rack-level reliability. Especially in environments where multiple power feeds, high outlet density, or frequent reconfigurations are common, visual differentiation helps prevent mistakes before they happen.
When evaluating PDUs, consider whether the outlet layout makes it easy to trace connections and organize cable paths. Some PDUs offer basic labeling, while others—like —go further by including color-coded outlets tied directly to associated breakers.
Introducing eConnect® PDUs with QuadLock Outlets: One Solution for All the Above
CPI’s latest innovation can help eliminate all these outlet-level pain points in one move.
Meet the new —this first-of-its-kind PDU that brings together everything you need for flexible, secure, and high-performance power distribution—all in one unit.
✅ Four-in-One Outlet Compatibility: Each outlet is compatible with C13, C15, C19, and C21—no adapters required.
✅ Built-In Locking Mechanism: Keep standard power cords securely connected – no clips, custom cables, or proprietary power cords required.
✅ High-Power Support: Deliver up to 57.5 kW per cabinet and support inputs up to 100A for AI and GPU-heavy workloads.
✅ Color-Coded Outlets: Simplify load balancing and speed up troubleshooting with clear visual organization.
✅ Modular and Scalable Design: QuadLock outlets are available across CPI’s entire eConnect PDU portfolio and can be pre-installed in CPI cabinet systems to streamline deployment.
See it in action: Watch the video below to get a closer look at how QuadLock works and what makes it different: