The difference between a reliable telecom room and one that underperforms? It comes down to the decisions made before a single rack goes in. One overlooked detail in the planning process can lead to costly retrofits and long-term inefficiencies.
And now—with AI workloads driving up thermal and power demands—there’s even less room for error. Supporting more compute requires precise planning across power, cabling, and cooling.
At Chatsworth Products (CPI), we’ve been in the trenches with IT and facilities teams and seen where telecom room design falls short. More importantly, we’ve helped organizations build reliable, scalable spaces that perform.
Here’s our guide to designing a telecom room that supports your goals—now and in the future.
Step 1: Build with Future Needs in Mind
It’s easy to dive into equipment needs and layout logistics—but before any racks go in, it’s worth taking a step back. The most reliable telecom rooms are built on thoughtful planning that accounts for operational and business needs.
Clarify the Room’s Role Early
If in-house IT teams will primarily use the space daily, ease of access and maintenance should be top priorities. If clients or partners will see the space, aesthetics might play a larger role. Clearly defining the room’s purpose from the start ensures it meets both technical and business needs.
Plan for Growth from Day One
A space that’s “just right” today may be overloaded tomorrow. To avoid airflow issues and cable congestion, leave at least 30% headroom for future equipment. It’s also smart to reference BICSI and TIA standards for space clearances and pathway design—they help ensure long-term functionality and serviceability.
Color Finish is More Than a Design Choice
Finish color might seem like a cosmetic detail, but it has real functional impact on performance. Opting for white racks or cabinets from the start enhances visibility and can reduce the need for additional lighting—especially in rooms with limited natural light. It also helps technicians more easily identify labels and connections. Making this decision early on helps you avoid the cost and disruption
Step 2: How to Choose the Right Rack or Cabinet for Your Telecom Room
The right rack or cabinet does more than meet spec—it simplifies cabling, supports airflow, and lays the groundwork for long-term scalability. The right choice depends on your equipment type, load, available space, and access requirements.
Rack/Cabinet Considerations
- are ideal for lightweight gear like patch panels and switches. They're space-efficient and budget-friendly—but may require added bracing or cable support as density increases.
- provide better weight distribution and stability for deeper equipment like servers or UPS systems. Look for models with adjustable mounting rails to simplify installation and future changes.
- – If floor space allows, cabinets provide the most protection, airflow control, and can include built-in cable management—especially useful when physical security or aesthetics are a concern.
Additional Features to Consider
- Built-in grounding and bonding eliminate the need for separate kits and helps streamline compliance.
- Higher usable U-space () gives you more room to grow within the same footprint—something easy to overlook but valuable in tight telecom rooms.
- Pre-included mounting hardware can save time and eliminate last-minute procurement headaches.
- Aluminum frames offer a strong yet lightweight alternative to steel—easier to maneuver during install and more cost-effective to ship.
Access & Security
If non-IT staff or third-party vendors will enter the room, cabinets with perforated locking doors can provide airflow and . For highly regulated industries, consider electronic locking solutions that track access attempts and support compliance requirements.
Step 3: How to Ensure Reliable Power in Network and Telecom Rooms
As telecom rooms evolve to support more active equipment—and in some cases, AI-capable hardware— your power strategy can determine whether the room supports growth or holds it back.
Build Resilience with the Right UPS
In many telecom rooms, switches and other networking gear are the first point of failure during a power event. Don’t stop at basic backup. A well-matched UPS should protect key devices, enable graceful shutdowns, and integrate into your monitoring systems.
Key considerations:
- Prioritize backup for distribution switches and networking gear that impact multiple systems.
- Choose compact UPS form factors (wall- or rack-mounted) to preserve usable rack space.
- Look for integration with PDUs or monitoring software so runtime, load, and health are visible in one place.
Design power delivery for visibility—not just capacity.
Intelligent PDUs go beyond delivery—they offer that help prevent overloads and track energy usage.
Look for:
- Granular data: Outlet-level monitoring helps pinpoint energy-hungry devices and identify ghost loads that silently consume power.
- Customizable thresholds and alerts: to catch overloading or imbalance before it causes downtime.
- Remote access to view loads, check breaker status, and reset devices in distributed sites without rolling a truck.
Step 4: Telecom Room Cooling Best Practices
Telecom rooms have evolved into high-performance spaces filled with active gear—and that means rising thermal loads. Even if your room runs cool now, future density could change that. Here’s how to stay ahead of the heat:
Ensure Proper Ventilation
At a minimum, your telecom room should have proper ventilation—air coming in and going out. Without basic airflow, you risk overheating even a modest amount of active equipment.
Plan for Growth with Dedicated Cooling
Consider a dedicated air conditioning unit for the telecom room. This allows you to control the temperature independently of the rest of the building, ensuring the room is optimized for equipment—not people. This is especially important if you're deploying switches or other electronics that generate heat. Just make sure the AC system is properly configured to exhaust air out of the room.
If you need to install a small number of heat-generating devices, consider sealed enclosures with integrated cooling. For example, support active cooling with options to safely vent exhaust, making them ideal for retrofits in non-conditioned environments.
Use Cabinets to Improve Efficiency
Open racks are harder to cool efficiently. Enclosed cabinets allow you to isolate airflow using blanking panels, brush strips, and ducting. This ensures cold air reaches equipment—and return air stays separate, improving overall thermal performance.
Step 5: Cable Management Tips for Efficient Telecom Room Design
Cable management isn't just about aesthetics—it’s about structure, efficiency, and operational resilience. Good management prevents pinch points, maintains signal integrity, and makes MACs smoother and more efficient.
Here’s how to avoid the usual pitfalls:
Size for Growth—Early and Accurately
One of the most common mistakes in telecom rooms is underestimating future cable volume. Without considering cable fill ratios or leaving room for expansion, racks can become overstuffed within a year or two—making cable management a nightmare and compromising airflow.
Use to size vertical managers and runways based on real projections.
Additionally, be sure to size both your cable managers and runways for the long term. Pay attention to width and height of your cable managers: when real estate is limited, you’ll want to make the most of vertical space.
Match the Manager to the Cable Type:
Not all cable managers are built the same. The right one depends on what you’re routing—and how much flexibility you need.
- For high-density copper: Use a tool-less, finger-style cable manager like CPI’s to support clean, flexible routing.
- For fiber or mixed environments: Choose a solution with integrated accessories and bend-radius control—like CPI’s which includes pre-installed doors, built-in routing features, and thoughtful design details to protect signal integrity and reduce packaging waste.
Use Runways for Clean Transitions
In real-world telecom rooms, cable entry and exit points rarely line up perfectly with your racks or cabinets—and rigid runway systems can lead to awkward routing, added install time, or costly workarounds.
That’s why we recommend CPI’s —a flexible solution with features designed to adapt to your space:
- Movable cross members let you fine-tune alignment over racks, cabinets, or cable entry points—no cutting or custom brackets required.
- Radius drops preserve bend integrity, protecting cable performance and longevity.
- Flexible mounting options support cables from ceilings, floors, or cabinet tops.
- UL Classified to meet grounding requirements where applicable.
- Ships assembled or unassembled to fit your install schedule and logistics.
Reminder: Improper installation of your cable runway—such as mounting runways upside-down or skipping bonding—can lead to signal interference or safety hazards.
Common Telecom Room Mistakes That Can Cost You Time and Money
Even experienced teams run into trouble when telecom rooms aren’t designed with long-term realities in mind. Here are the biggest pitfalls we see—and how to avoid them before they cost you time, money, or performance.
1. Underestimating Space and Growth Trajectory
It’s not just about what fits today—it’s what won’t fit next year. Expansion isn’t always an option and as equipment densities rise and MACs pile up, rooms that once felt spacious quickly become limiting.
How to avoid it:
- Right-size your room early, based on realistic growth projections.
- Use taller racks or higher-density configurations to make better use of vertical space.
- In space-constrained environments, modular or custom rack systems (like those offered by CPI) can help you squeeze more value from every square foot.
2. Poor Access Planning
Oftentimes equipment can’t make it through the door. Too many telecom rooms are built without considering how hardware will be moved in, out, or around the space.
How to avoid it:
- Plan access points as early as rack layouts.
- Use double-door entries or oversized pathways to accommodate full-size cabinets, future upgrades, and emergency equipment replacements.
3. Overlooking Compliance
Overlooking BICSI or TIA standards leads to poor airflow, overcrowded racks, and risk exposure you can’t afford.
How to avoid it:
- Design to and to future-proof your environment.
- Select racks and cable management systems to meet both regulatory and performance needs.
4. Not Planning for Ongoing Maintenance
Even the best-designed telecom room won’t perform well without regular upkeep. Dust buildup, cable sprawl, and unmonitored hardware gradually turn a high-performance space into a liability.
How to avoid it:
- Establish a maintenance schedule with clear ownership.
- Periodically inspect for airflow obstructions, tangled cables, or hardware issues before they become failures.
- Routine cleaning and reorganization can extend hardware life and reduce downtime risk.
Telecom Room Design Support: Get Expert Help from CPI
At CPI, we’ve worked with teams facing all these challenges—and helped them get back on track. From racks and cabinets to power, cooling, and cable management, are designed to support long-term performance in even the most space-constrained environments.
Need help? and get expert guidance tailored to your space, goals, and constraints.