AI and machine learning aren’t just for Silicon Valley anymore. Across colleges and universities, higher education IT teams are under increasing pressure to deliver more compute, faster speeds, and higher reliability—without compromising on sustainability or budget.
Whether you're standing up a new AI research lab, refreshing a legacy server room, or planning an edge deployment in a remote campus building, today’s demands are stretching yesterday’s cooling strategies to their breaking point.
So, here’s the question: How do you support increasingly powerful, high-density hardware in older, space-constrained environments—without ripping and replacing your entire infrastructure?
The Real Challenges You’re Solving For
Campus IT environments aren’t built like enterprise data centers—and your cooling strategy shouldn’t try to copy one.
You’re working within real-world constraints:
- Decentralized server rooms and research labs
- Legacy buildings that were never designed for high-density computing
- Tight budgets, tighter timelines, and a hard stop on downtime
- Increasing demand for AI and HPC support—this year, not next
- Leadership pressure to reduce energy use and demonstrate cost control
This isn’t just about cooling—it’s about preparing your infrastructure for the next era of digital learning and research. And liquid cooling is quickly emerging as the most efficient, scalable way forward.
How Do You Know When Air Cooling Has Reached Its Limits?
If you’re even asking, you probably already have hit the limit. The signs aren’t always dramatic, but they’re impossible to ignore:
- You’re consistently exceeding rack power densities of 20 kW or higher
- Airflow optimizations aren’t delivering meaningful performance gains
- Your facility’s physical limitations—floor space, ceiling height, airflow capacity—are becoming bottlenecks
- You’re under pressure to meet sustainability goals or carbon reduction targets
If your institution is investing in AI, research computing, or next-gen infrastructure, liquid cooling isn’t just worth it—it’s the infrastructure that makes everything else possible.
Is It All-or-Nothing? Or Can We Start Small?
It’s one of the most common questions—and a good one. Liquid cooling sounds like a big shift, but not all systems are the same. The truth is, you can absolutely start small and scale at your own pace—if you choose the right approach.
There are several types of liquid cooling technologies, each with varying complexity:
- Rear-door heat exchangers: These replace the back door of a cabinet to transfer heat using chilled water. Effective, but typically require integration with facility-level water systems.
- Immersion cooling: Servers are fully submerged in non-conductive liquid. High-performance, but not ideal for retrofit or modular use cases.
- Direct-to-chip cooling: Delivers coolant directly to the processor using cold plates for highly targeted cooling. Systems may use single-phase fluid, which stays liquid throughout the process, or two-phase dialectic fluid, which changes to a vapor to absorb even more heat.
Why Direct-to-Chip Stands Out for Higher Ed
Direct-to-chip systems—especially closed-loop, waterless designs—offer the best balance of performance, flexibility, and simplicity. They’re ideal for:
✅ Starting small—deploy in a single cabinet, lab, or server room without modifying your entire facility
✅ Avoiding infrastructure disruption—no external plumbing, no major construction
✅ Scaling over time—expand capacity only as needed, in line with your growth
This gives IT teams the control to modernize gradually, without overcommitting or overspending. It’s smart, adaptive infrastructure that moves at the pace of your institution.
A Scalable Solution That Fits Higher Ed's Needs
At Chatsworth Products, we’ve combined our expertise in cabinet engineering with ZutaCore’s revolutionary two-phase liquid cooling technology to deliver a fully integrated, turnkey solution—built specifically for high-density, campus IT environments.
ZetaFrame® + ZutaCore®: A Turnkey, High-Density Cooling Solution
Here’s how it works:
- We start with the ZetaFrame® Cabinet System, engineered for optimal airflow, and integrated components such as power management, cable management, access control and more—all factory integrated.
- We pre-integrate the ZutaCore® HyperCool® waterless, direct-to-chip, two-phase liquid cooling—extracting the heat at the source, removing up to 2800W per chip.
- We assemble, configure, and test the entire system before it ever leaves our facility—ensuring it arrives on your campus fully functional and deployment-ready.
The result?
A complete, high-density liquid cooling cabinet that’s shipped to you as a single, ready-to-roll unit. No delays. No surprises. Just plug it in, power it up, and get to work.
Why It Works So Well in Higher Ed
This system is especially well-suited for education environments because it’s:
- Closed-loop and waterless – Less risk of damage to electronics
- Optimized for AI, HPC, and GPU-intensive workloads – Ready for what’s next
- Deployable anywhere – No need for mechanical overhauls or specialized spaces
- Energy-efficient by design – Helps meet institutional ESG and carbon goals
See It in Action:
Schedule a quick consultation to explore how the ZetaFrame® + ZutaCore® system could transform your IT environment—without overhauling your entire campus.
Want Help Making the ROI Case?
Not sure how to justify the investment internally? We’ve got you covered.
We offer complimentary CFD (Computational Fluid Dynamics) modeling to help you clearly visualize airflow challenges, thermal performance, and potential energy savings—all tailored to your unique environment and goals. Contact us here to get started.
Interested in how the ZetaFrame® and ZutaCore® solution could work for you?
Schedule a free consultation and let’s explore what’s possible.