It’s easy to treat “seismic-rated” as a box to check—a requirement tied to building codes and inspections. But in practice, seismic ratings have far greater implications for how data center and IT infrastructure performs when conditions are far from normal.
A seismic-rated rack or enclosure isn’t just about meeting minimum requirements. It’s about how equipment behaves under motion, how predictable that behavior is, and how quickly systems can recover once the event passes. Understanding that difference is key to making more resilient infrastructure decisions.
Designed for Motion, Not Just Weight
At its simplest, a seismic-rated rack or enclosure is designed and evaluated to withstand earthquake forces—not just support equipment under static conditions.
Most standard racks are built for environments where equipment stays still. There’s no acceleration, no side loading, and no sudden directional change. During an earthquake, those assumptions disappear.
Seismic-rated racks are designed for dynamic motion, including:
- Side-to-side movement
- Front-to-back sway
- Vertical acceleration
In other words, they’re built for what actually happens during a seismic event—not for ideal conditions on paper.
Seismic-Rated vs. Non-Seismic: A Difference in Design Intent
Non-seismic racks can be installed in seismic regions, but they rely heavily on external engineering measures—anchors, bracing, and reduced equipment loads—to compensate for limitations in the rack itself. Their performance depends largely on site-specific engineering and installation quality, and they are more susceptible to secondary damage during an event.
Seismic-rated racks are designed differently from the start. Reinforced frames and structural bracing help manage motion and reduce the transfer of vibration to installed equipment. When properly evaluated, these racks behave more predictably under stress and often support higher usable equipment capacity during a seismic event.
That difference in design intent is what allows seismic-rated racks to support both compliance and operational resilience.
Are Seismic-Rated Racks Required?
This is one of the most common questions—and the answer is nuanced.
Building codes generally require non-structural components, such as racks and cabinets, to be properly supported and restrained in seismic regions. They do not always mandate a specific rack type. However, expectations change in environments where continued operation matters.
Facilities expected to remain operational during and after an earthquake, sites with dense or mission-critical equipment, and environments where downtime poses safety, financial, or public-service risks often specify seismic-rated racks. In these cases, the decision isn’t about checking a regulatory box—it’s about reducing risk and improving post-event operability.
Understanding Seismic Load Ratings
Load ratings are another area where compliance and performance are often confused.
Static load ratings describe how much weight a rack can support when nothing is moving. Seismic load ratings describe how much equipment a rack can support while undergoing seismic motion. Because earthquakes introduce acceleration and directional change, seismic load ratings are typically lower than static ratings—unless the rack is specifically engineered to manage those forces.
This distinction matters because seismic load ratings determine how much equipment can be installed per rack in a seismic region, directly affecting floor efficiency and overall infrastructure design.
How Seismic Performance Is Evaluated
Not all seismic claims are supported by the same level of evidence.
Some racks are evaluated primarily through engineering calculations, while others undergo physical testing that simulates earthquake motion. Shaker table testing, for example, subjects racks to controlled motion profiles and evaluates whether they maintain structural integrity and functionality under dynamic conditions.
For buyers and specifiers, the key takeaway is straightforward: documentation matters. A credible seismic rating should be supported by test reports, certifications, or engineering data—not just a label.
How CPI Supports Seismic-Ready IT Infrastructure
Based in Southern California—one of the most seismically active regions in North America—Chatsworth Products (CPI) has long designed racks and enclosures with seismic performance in mind.
Rather than relying on a single benchmark, CPI evaluates seismic performance against multiple recognized standards and uses third-party validation to understand how different testing methods compare under real-world conditions. This approach helps ensure that seismic claims are defensible, documented, and appropriate for the application.
Explore CPI’s and or to discuss your specific seismic requirements and facility needs.