Deploying Wi-Fi 7 wireless access points is not just a technical task but a strategic initiative that influences network performance, physical security, aesthetics, adaptability, and manageability throughout the installation's life cycle.
A well-planned deployment can enhance performance, streamline maintenance, and reduce future upgrade costs.
Here’s what you need to consider when installing Wi-Fi 7 access points.
Key Tips for Deploying Wi-Fi 7 Access Points Effectively
As Wi-Fi 7 access points become more advanced, they’re also becoming larger and heavier—making secure, long-term installation more important than ever. Simply clipping APs onto ceiling grids is no longer ideal, especially in environments that require modern functionality and aesthetics.
There’s also a growing emphasis on preserving architectural design. Whether maintaining the character of a historic building or complementing the sleek look of a modern space, it’s important to choose an installation method that allows APs to blend seamlessly into their surroundings.
Here are a few tips for more effective AP deployment:
- Optimize AP positioning. Mount access points where they can deliver the best coverage and performance.
- Ensure rapid serviceability. Choose mounting solutions that support fast access and maintenance to reduce time and labor costs.
- Improve physical security. Use enclosures or mounts that deter costly tampering and unauthorized access.
- Provide a low-cost migration path. Select systems with interchangeable doors and trims to reduce time in the space, material cost to upgrade, and overall project cost.
- Support healthcare environments. Opt for solutions that simplify infection control procedures and help reduce compliance-related expenses.
- Standardize across the facility. A consistent installation look and functionality will help reduce reduces maintenance costs, tool requirements, and operational processes.
Industry Best Practices: Guidelines from ANSI/BICSI 008-2024
to ensure long-term network efficiency, cost-effectiveness, and seamless operational support:
- “The wireless access point infrastructure physical design should consider consistency, compatibility, and ease of operational support while lowering overall cost.”
- “Design costs should consider both initial installation costs as well as operational costs.”
- “Ease of operational support and consistency.”
Strategic Access Point Deployment Ensures Long-Term Success
The foundation of any successful network begins with the installation of wireless access points (APs). By strategically optimizing your AP installation platform, you can not only meet current performance, security, and network operational requirements but also ensure the network is prepared for future deployments and advancements. This approach supports long-term efficiency, scalability, and adaptability as technology continues to evolve.
To achieve this, choosing the right installation solutions is essential. Let’s explore the options that can help you deploy Wi-Fi 7 APs effectively while meeting the evolving demands of modern environments.
Wi-Fi 7-Ready Access Point Mounts and Enclosures
Oberon® offers wireless installation mounting solutions designed specifically for the integration of wireless network edge components into any environment, from indoor ceiling and wall mounting to outdoor, facilitating compliance with industry guidelines, and recommendations.
: A Modern Approach to Ceiling Mounting Equipment
Model 1047 Series:
- 2’ x 2’ ceiling tile enclosure offering interchangeable doors
- Sophisticated modern design seamlessly blends into the ceiling structure with attractive textured powder coat finish
- Lockable drop-down doors permit quick and easy access to equipment and cabling WITHOUT the need to open the above ceiling space
- Mounts AP flush to the ceiling, with an AP specific door for optimal wireless coverage
- Solid back-box fills opening behind AP in the ceiling creating an effective fire-resistant, smoke and dust barrier simplifying ICRA compliance
- Firestop grommet to properly seal cable egress in the backbox
- Stow service loop cable and connectivity components in the backbox
- UL 2416 listed for low voltage applications. Designed to meet NEC300-22 and 300-23 for plenum installations. OSHPD approved, OPM-0110-13
- Constructed to be compliant with City of Chicago Environmental Air (CCEA) plenum requirements
: A Modern Approach to Horizontal Wall Mounting
Model 1011:
- Modern design mounts the Wi-Fi AP in preferred horizontal orientation on walls with a professional finish
- The universal design accommodates most manufacturer wireless APs
- The opening in the back enables installation directly over a telecommunications outlet
- Secure cover conceals outlet, connectors, and cabling knockouts on two sidewalls for 1 in. trades size conduit connectors
- Ideal for High-Traffic Areas – Suitable for campuses, transportation hubs, smart city deployments, business parks, and recreational spaces.
- Outdoor-Ready Protection – Constructed from rugged, weather-resistant materials to protect wireless equipment from environmental elements.
- Secure, Concealed Equipment Housing – Shields access points and networking components from vandalism and unauthorized access.
- Aesthetic, Low-Profile Design – Blends into outdoor landscapes while discreetly housing wireless infrastructure.
Future-Proof Your Wi-Fi 7 Network with the Right Deployment Solutions
Wi-Fi 7 is poised to be a game-changer in wireless technology. Expanding on the foundation of Wi-Fi 6/6E, it brings significant enhancements in channel bandwidth, modulation techniques, and the ability to handle multiple devices more effectively.
Modernizing your wireless AP deployment will enhance your network's operational efficiency, meet aesthetic and performance goals, and simplify management requirements.
today and discover how the right installation can maximize your network’s performance and longevity.