As AI workloads continue to push rack densities beyond what traditional air cooling was designed to handle, conversations around liquid cooling have accelerated. But despite the growing attention, hybrid cooling remains one of the most misunderstood approaches in the modern data center.
Hybrid cooling works best when it is viewed as part of a broader physical infrastructure strategy. Cabinets, power distribution, airflow management, cable management, containment, and monitoring all contribute to thermal performance—and each becomes more important as rack densities increase.
Rather than replacing air cooling entirely, hybrid cooling combines liquid and air technologies to manage heat more efficiently while allowing organizations to evolve their infrastructure over time. The conversation isn't simply about cooling technology—it's about building physical infrastructure that can adapt as AI deployments continue to grow.
Here are 10 facts that may surprise you.
1. Most AI deployments still rely on air cooling.
While headlines often focus on direct-to-chip liquid cooling, most enterprise AI environments continue to use a combination of air and liquid cooling. Hybrid approaches allow organizations to support higher-density racks without redesigning the entire data center.
2. You don't have to convert your entire data center.
One of the biggest misconceptions is that adopting liquid cooling requires a facility-wide overhaul. Many organizations begin with a handful of high-density AI racks while the remainder of the data hall continues using traditional air cooling. This phased approach allows operators to scale AI infrastructure as demand grows instead of making an all-or-nothing investment.
3. Hybrid cooling isn’t just for hyperscalers.
Many organizations assume hybrid cooling only makes sense in massive AI campuses or hyperscale data centers. Enterprises, healthcare organizations, higher education, government agencies, research institutions, and colocation providers are increasingly adopting hybrid cooling as they introduce higher-density AI workloads into existing facilities.
Because hybrid cooling can be deployed selectively—cooling only the racks that need it—it provides a practical path for organizations that want to support AI without redesigning their entire data center.
4. The cabinet has become a critical part of the cooling strategy.
As compute densities increase, the cabinet becomes more than a place to mount equipment. Rather than locking organizations into a single architecture, today's infrastructure should accommodate evolving IT equipment, changing cooling technologies, and future expansion with minimal disruption. It must support higher weight capacities, intelligent cable routing, scalable power distribution, effective airflow management, and compatibility with rack-level cooling technologies—all while remaining easy to deploy and service. The rack-level infrastructure surrounding the IT equipment has become just as important as the cooling technology itself.
5. Higher density doesn't automatically mean higher efficiency.
Packing more compute into a rack can improve utilization, but only if power delivery, cooling, airflow, and cable management are designed as a complete system. Otherwise, hotspots, stranded capacity, and operational inefficiencies can offset the benefits of higher density.
6. Retrofitting is often possible.
Many existing facilities can accommodate hybrid cooling with targeted infrastructure upgrades rather than complete replacement. Improving airflow management, implementing containment, optimizing cable pathways, and adding rack-level cooling where needed can significantly increase cooling performance while extending the useful life of existing infrastructure. Choosing infrastructure that simplifies installation and future modifications can reduce deployment time while making ongoing expansion less disruptive.
7. Cable management affects cooling performance.
Poor cable routing can obstruct airflow, making both air- and liquid-cooled environments less efficient. As rack densities increase, disciplined cable management becomes an important part of thermal management—not just organization. Maintaining clear airflow paths helps maximize the effectiveness of every cooling strategy.
8. Monitoring matters more than ever.
Hybrid cooling introduces additional variables that operators need to understand. Power utilization, environmental conditions, and cooling performance should all be monitored continuously to maximize available capacity, improve operational visibility, and identify potential issues before they become downtime events.
9. Every workload doesn't need the same cooling strategy.
Not every rack requires liquid cooling. Many data centers will operate mixed-density environments for years, with some cabinets requiring advanced cooling while others continue operating efficiently with optimized air cooling. Even in liquid-cooled environments, network equipment, power distribution, and many IT systems will continue to rely on effective airflow management. Infrastructure that supports this flexibility gives organizations more options as technology evolves.
10. Hybrid cooling is really about flexibility.
Perhaps the biggest surprise is that hybrid cooling isn't simply a cooling strategy—it's an infrastructure strategy. It enables organizations to deploy AI where it makes business sense, support a mix of cooling technologies, and scale over time without rebuilding the entire data center. Investing in adaptable physical infrastructure today helps organizations support multiple generations of IT technology without repeated infrastructure redesigns.
Preparing for What's Next
The future of data center cooling isn't likely to be all air or all liquid. For many organizations, it will be a thoughtful combination of both.
Organizations that build flexibility into their physical infrastructure—from cabinets and cable management to power distribution, airflow management, and rack-level cooling—will be better positioned to support future AI workloads without unnecessary disruption.
As cooling technologies continue to evolve, adaptable infrastructure will remain one of the smartest long-term investments a data center can make. The organizations that will adapt the fastest to tomorrow's AI infrastructure won't necessarily be those with the newest facilities—they'll be the ones that designed flexibility into their infrastructure from the beginning.