Getting the power architecture right for 30–100 kW AI racks directly determines whether your facility can deliver its intended compute capacity—or whether stranded power, thermal bottlenecks, and monitoring blind spots limit infrastructure utilization and future scalability.
The good news is that most organizations don't need to redesign everything at once. A well-planned power architecture allows facilities to scale from today's high-density deployments to tomorrow's even higher rack loads while minimizing stranded capacity and avoiding expensive rework.
Here's what to consider when designing a power architecture for modern AI deployments.
Why 30–100 kW Is a Different Engineering Problem
For many organizations, the jump from traditional enterprise racks to 30–100 kW AI racks isn't simply a matter of adding more power. It fundamentally changes how the rack—and the surrounding infrastructure—must be designed.
At these densities, decisions about power distribution, cabinet layout, cable management, airflow, monitoring, and cooling become tightly interconnected. A change in one area often affects every other. For example, adding higher-capacity PDUs may require different cable routing, which can influence airflow and serviceability. Similarly, increasing rack power density raises heat loads, affecting cooling strategy and future expansion plans.
Many organizations reach this range while retrofitting an existing data center or deploying AI within a colocation environment, where available power and space are already constrained. That makes thoughtful infrastructure planning even more important. Rather than treating power as a standalone electrical project, successful AI deployments take a system-level approach that considers how every layer of the physical infrastructure works together.
Understanding these interactions is the first step toward building a power architecture that can support today's AI workloads while remaining flexible enough for the next generation of higher-density compute.
Start with the End State, Not Today's Load
Many AI deployments begin with a handful of GPU racks. Within a year, that pilot often grows into an entire row—or multiple rows—of high-density cabinets.
Designing infrastructure around today's requirements can create bottlenecks later.
Instead, begin by asking questions such as:
- What rack densities are expected over the next three to five years?
- Will workloads continue increasing beyond 30 kW?
- Could certain rows eventually require liquid cooling?
- How much expansion capacity should be reserved?
Organizations planning for higher rack densities may also need to evaluate when air cooling reaches its practical limits.
Planning around the future state helps prevent costly infrastructure changes after equipment is deployed while reducing the risk of stranded capacity and future redesigns.
Power Distribution Must Scale with Density
Power distribution becomes increasingly complex as rack densities climb.
Higher-density deployments often require:
- Higher-amperage branch circuits
- Increased circuit redundancy
- Larger conductor sizes
- Flexible PDU configurations
- Standardized power distribution across global deployments
For many AI environments, traditional 20A branch circuits are no longer sufficient. Thirty-amp circuits are increasingly becoming the practical baseline for supporting modern GPU infrastructure while maintaining operational flexibility.
Understanding how rack power requirements are calculated is an important first step in selecting the appropriate power architecture.
Equally important is selecting intelligent PDUs that provide accurate power monitoring, outlet-level visibility where appropriate, and the flexibility to support changing equipment configurations over time.
Rather than viewing PDUs as simple power strips, organizations should consider them a critical source of operational data that informs capacity planning and day-to-day management.
Treat the Rack as Part of the Power System
One of the biggest mistakes organizations make is viewing the cabinet as simply a place to mount equipment. The cabinet becomes an active part of the power architecture.
High-density AI deployments require cabinets capable of supporting:
- Large numbers of high-current power cords
- Multiple high-capacity PDUs
- Increased cable volume without restricting airflow
- Equipment weight that can exceed traditional enterprise deployments
- Integrated environmental and power monitoring
At 30–100 kW, physical infrastructure decisions directly influence deployment speed, serviceability, and long-term reliability.
This is why AI-ready cabinets are designed as infrastructure platforms rather than passive enclosures. When cabinets, power distribution, cable management, airflow management, and monitoring are designed together from the outset, organizations can simplify deployment, reduce integration challenges, and create a more repeatable infrastructure standard across AI environments.
Design for Monitoring from Day One
As rack densities increase, so does the cost of uncertainty. Without accurate monitoring, organizations often:
- Overprovision available capacity
- Leave usable power stranded
- Miss developing electrical issues
- Delay new deployments because available capacity cannot be confidently verified
A modern power architecture should include continuous visibility into:
- Circuit utilization
- Phase balancing
- PDU load
- Environmental conditions
- Capacity trends over time
This operational intelligence enables facilities teams to maximize existing infrastructure while reducing operational risk.
For AI deployments, monitoring is no longer simply an operational tool—it becomes an essential design element that enables informed capacity planning, proactive maintenance, and confident infrastructure expansion.
Cooling and Power Can No Longer Be Designed Separately
Every kilowatt consumed eventually becomes heat that must be removed.
That means power planning and cooling planning are inseparable.
A rack operating at 40 kW creates a dramatically different cooling requirement than one operating at 10 kW. As densities approach 60–100 kW, organizations often begin evaluating hybrid or liquid cooling strategies for portions of the deployment.
Designing the power architecture without considering future cooling requirements can limit upgrade options later.
Instead, organizations should coordinate cabinet selection, power distribution, airflow management, containment, and cooling strategies as a single integrated design.
This system-level approach reduces rework as AI infrastructure continues to evolve.
Design for Repeatability, Not Just Capacity
One lesson repeated across hyperscale, colocation, enterprise, and research environments is that standardization improves both deployment speed and operational consistency.
Rather than creating unique cabinet configurations for every deployment, organizations benefit from establishing repeatable infrastructure standards.
Standardization can include:
- Common cabinet platforms
- Consistent PDU configurations
- Standard branch circuit designs
- Uniform cable routing practices
- Shared monitoring architecture
These repeatable designs simplify installation, reduce operational variability, and make future expansion significantly easier.
This engineering discipline becomes increasingly valuable as AI deployments scale across multiple facilities.
Common Power Architecture Mistakes to Avoid
Organizations planning for 30–100 kW AI racks often focus on delivering enough power but overlook the infrastructure decisions that determine long-term scalability and reliability. Watch for these common pitfalls:
Treating power distribution as a standalone project.
Power architecture cannot be separated from cabinet design, cable management, cooling, and monitoring. Decisions in one area affect performance and serviceability across the entire rack.
Designing only for today's power density.
AI hardware continues to push rack power requirements higher. Building infrastructure with no room for growth can lead to costly upgrades sooner than expected.
Waiting to implement monitoring.
Without real-time visibility into power utilization and environmental conditions, it's difficult to accurately plan capacity, identify emerging issues, or confidently deploy additional equipment.
Selecting individual components instead of designing an integrated system.
Cabinets, PDUs, cable management, airflow management, and cooling should be engineered to work together. A coordinated infrastructure strategy reduces deployment risk, simplifies expansion, and improves operational consistency.
The common thread behind each of these challenges is that successful AI infrastructure isn't built one component at a time. It requires an integrated approach to power, cooling, cabinet design, cable management, and monitoring.
The most resilient AI infrastructure isn't built by optimizing individual components—it's built by engineering the interactions between power distribution, cabinets, cable management, airflow management, cooling, and monitoring.
Why CPI Designs Power Architecture as an Integrated System
Power architecture isn't built by selecting individual components in isolation.
The most successful AI deployments begin with an understanding of how cabinets, power distribution, airflow management, cooling, cable management, and monitoring work together.
That's why CPI approaches high-density infrastructure as an integrated system rather than a collection of independent products.
An AI-ready cabinet supports more than equipment installation. It provides the foundation for scalable power distribution, cable management that preserves airflow, intelligent power monitoring, and future cooling strategies as rack densities continue to increase.
For many deployments, integrating these infrastructure elements before the cabinet reaches the data center can reduce installation variability, simplify commissioning, and help accelerate time to deployment.
Likewise, intelligent eConnect® PDUs provide both reliable power distribution and the operational visibility needed to safely manage high-density environments over time. Combined with airflow management and containment solutions, organizations can build infrastructure that adapts as AI workloads evolve instead of requiring major redesigns every few years.
This systems-based engineering approach helps reduce deployment risk while creating infrastructure that remains flexible as technologies and power requirements continue to change.
Build for the Next Generation of AI
Building a power architecture for 30–100 kW AI racks isn't simply about delivering more electricity to a cabinet. It's about designing infrastructure that can evolve as AI workloads, power densities, and cooling requirements continue to change.
It's about creating a scalable infrastructure foundation that balances power distribution, monitoring, cooling, serviceability, and future growth.
The goal isn't simply to support a 30 kW, 60 kW, or even 100 kW rack. It's to build an infrastructure architecture that can adapt as power densities, cooling technologies, and AI hardware continue to evolve.
Related reading:
- High-Density Power Infrastructure: What Changes for AI Deployments?
- How Much Power Does an AI Rack Use?
- Why High-Density AI Racks Are Becoming the Standard for Modern AI Infrastructure
- When Do You Need Liquid Cooling for AI Infrastructure?
Download CPI's Powering AI Infrastructure white paper to explore engineering considerations for power distribution, monitoring, cabinet design, and scalable AI deployments.