As AI deployments continue to increase in density, many organizations are asking the same question:
When do you need liquid cooling?
The answer is not tied to a single rack density. While many organizations begin evaluating liquid cooling when rack densities approach 30 kW, the decision depends on several factors, including cooling capacity, airflow management, future growth plans, and operational risk.
For organizations new to liquid cooling, it's important to understand the different approaches available, from direct-to-chip systems to immersion cooling. Our guide to liquid cooling in data centers explores the major technologies, benefits, and deployment considerations in greater detail.
Modern air-cooled data centers can support higher densities than ever before. However, AI workloads are pushing power and thermal demands into territory where traditional cooling approaches become increasingly difficult to scale efficiently.
The better question is not whether air cooling still works—it is whether your current cooling strategy can continue supporting future AI growth without creating constraints.
Is There a Rack Density Threshold for Liquid Cooling?
One of the most common questions surrounding AI infrastructure is whether there is a specific rack density that requires liquid cooling.
The reality is that there is no universal threshold.
A well-designed data center with effective airflow management, containment, optimized cabinet design, and sufficient cooling infrastructure may support densities well beyond what many organizations consider possible with air cooling alone.
That said, many operators begin evaluating liquid cooling as rack densities approach 30 kW per cabinet. This is often the point where cooling strategy becomes a major planning consideration rather than simply an operational concern.
As densities move into the 40–50 kW range and beyond, liquid cooling becomes increasingly attractive because the amount of heat generated within the cabinet begins challenging the practical limits of air-based heat removal.
Rather than viewing these numbers as hard rules, they should be viewed as planning thresholds that help organizations assess whether their current infrastructure can support future growth.
How Far Can Air Cooling Be Pushed?
Air cooling remains an effective solution for many high-density environments.
Advancements in containment, airflow management, cabinet design, and environmental monitoring have allowed organizations to support workloads that would have required liquid cooling just a few years ago.
Several factors determine how far air cooling can be pushed:
- Cabinet airflow design
- Hot aisle or cold aisle containment
- Cable management practices
- Room cooling capacity
- Environmental monitoring
- Rack layout and spacing
When these elements are properly designed and managed, organizations can often support significantly higher densities without immediately transitioning to liquid cooling.
However, as density increases, cooling performance becomes increasingly dependent on precision. Small inefficiencies that have little impact at lower densities can create meaningful thermal challenges at higher densities.
What Are the Warning Signs That Air Cooling Is Reaching Its Limits?
Organizations often focus on rack density alone when evaluating cooling strategies. In practice, operational warning signs are often a better indicator that change may be needed.
Common indicators include:
Persistent Hot Spots
If certain cabinets or equipment consistently run hotter than surrounding infrastructure despite airflow adjustments, cooling capacity may be reaching its practical limit.
Cooling Becomes the Deployment Bottleneck
Many data centers still have available floor space and power capacity but cannot deploy additional equipment because cooling resources are exhausted.
Increased Fan Speeds and Energy Consumption
As cooling systems work harder to maintain acceptable temperatures, fan energy consumption increases and overall efficiency declines.
Uneven Thermal Performance
Large temperature differences between cabinets often indicate airflow limitations that become increasingly difficult to resolve as density grows.
Limited Capacity for Future Expansion
Even if current workloads operate successfully, organizations may find there is little remaining headroom to support additional AI deployments.
These warning signs often appear before temperatures become critical, making them valuable indicators for long-term planning.
Why AI Workloads Accelerate the Need for Liquid Cooling
Traditional enterprise applications typically distribute compute resources across multiple servers and cabinets. AI infrastructure often concentrates large amounts of compute power into a much smaller footprint.
GPU-intensive workloads generate substantial heat while operating at high utilization levels for extended periods. As more compute resources are packed into each cabinet, thermal loads increase rapidly.
This concentration changes the cooling equation.
Removing heat with air requires moving increasingly larger volumes of air through the cabinet and surrounding environment. Eventually, the airflow required becomes difficult to manage efficiently.
Liquid cooling addresses this challenge by removing heat much closer to the source, allowing organizations to support significantly higher densities without relying exclusively on increased airflow.
Different liquid cooling technologies accomplish this in different ways. For a broader overview of common liquid cooling approaches and where they fit, see our guide to liquid cooling in data centers.
For many AI deployments, liquid cooling is not adopted because air cooling has failed. It is adopted because liquid cooling provides a more scalable path forward.
Should You Wait Until Air Cooling Stops Working?
In most cases, the answer is no.
Waiting until cooling becomes a critical constraint can limit deployment flexibility and increase project complexity. Infrastructure planning cycles are often measured in months or years, while AI demand can grow much faster.
Organizations evaluating liquid cooling should consider:
- Expected AI growth over the next three to five years
- Available cooling capacity
- Space constraints
- Power infrastructure plans
- Operational efficiency goals
- Future rack density requirements
Many organizations are now assessing liquid cooling well before reaching hard thermal limits. This proactive approach provides greater flexibility and allows cooling strategies to evolve alongside AI adoption.
The Right Time to Evaluate Liquid Cooling
There is no single rack density that automatically requires liquid cooling.
However, once AI deployments begin pushing toward higher densities, cooling strategy becomes a critical part of infrastructure planning.
For many organizations, the evaluation process begins around 30 kW per cabinet and becomes increasingly important as densities continue to rise. The decision should be based not only on current requirements but also on future growth, operational efficiency, and long-term scalability.
Understanding the available cooling technologies is an important next step. Learn more about the types of liquid cooling systems used in modern data centers, along with their benefits and deployment considerations.
The goal is not simply to determine whether air cooling still works. The goal is to ensure your infrastructure can continue supporting AI workloads without creating thermal constraints, stranded capacity, or unnecessary operational risk.
As AI deployments continue to evolve, organizations that proactively evaluate cooling strategies will be better positioned to scale efficiently and support the next generation of high-density workloads.