For decades, standard data center infrastructure—server racks, cabinets, and containment—has been the foundation of efficiency. Predictable form factors and repeatable designs kept costs under control. But as densities rise and deployment models diversify, standard racks and enclosures can no longer cover every scenario.
Key factors driving this shift include:
- Rising rack densities — AI and HPC workloads are now drawing 30–50 kW per rack, exposing thermal and power challenges that standard cabinet designs cannot always address.
- Constrained facilities — legacy buildings being retrofitted into modern IT spaces present unique ceiling heights, sprinkler layouts, and structural barriers.
- Distributed expansion — edge and industrial deployments place IT equipment in environments that were never designed for it, from factory floors to remote substations.
- Regulatory environments — cleanroom, healthcare, and financial facilities introduce compliance requirements that off-the-shelf products cannot always meet.
These are becoming mainstream scenarios as the industry diversifies. Forcing standard racks or containment into unsuitable environments results in inefficiency, stranded capacity, and higher operational risk.
Redefining Customization for Data Center Infrastructure
“Custom” has traditionally implied delays, inflated budgets, and one-off designs. That’s because many vendors treat it as an exception rather than a core capability.
Chatsworth Products (CPI) takes a different approach. For more than three decades, CPI has partnered with enterprises, colocation providers, healthcare networks, and hyperscale operators to address challenges standard solutions can’t solve—aligning custom infrastructure with the same deployment timelines expected of off-the-shelf products.
With more than 30 years of experience, CPI has made data center cabinet customization a core strategy, supported by:
- Dedicated customization team — engineers, designers, and documentation specialists whose sole focus is solving non-standard challenges.
- Advanced R&D facility — in-house labs where concepts can be designed, tested, and validated before deployment.
- Depth of customization — from small modifications (airflow baffles, tray adjustments) to ground-up cabinet systems built for unique industries such as semiconductors or healthcare.
- Nimble manufacturing — vertically integrated, ISO-certified plants that can move from prototype to production quickly, without the bottlenecks common in large OEM supply chains.
- Global manufacturing footprint: fast deployment support wherever infrastructure is needed.
This combination changes the equation: CPI can deliver tailored solutions with the speed, quality, and repeatability of standard products.
Real-World Customization Examples
If you're considering customization, these real-world examples demonstrate CPI has helped organizations across industries meet specific technical, regulatory, and operational needs.
Semiconductor: Cleanroom Compliance
Challenge: A semiconductor manufacturer required enclosures inside a cleanroom and sub-fab environment. Standard cabinets risked off-gassing and particle emissions that could jeopardize production.
Solution: CPI developed custom data center cabinets and containment systems engineered with low off-gassing materials and precision airflow management to comply with ISO cleanroom standards.
Hyperscale: Rapid Deployment at Scale
Challenge: A hyperscale cloud provider needed to scale quickly across multiple regions. Standard cabinet models slowed procurement and created complexity in logistics.
Solution: CPI created a custom server rack platform that could be ordered under a single part number, then adapted for site-specific requirements. This approach streamlined supply chain management and accelerated deployment timelines.
Healthcare: Custom Containment for UF Health Shands Hospital
Challenge: UF Health Shands Hospital needed a new 2,200 sq. ft. data center to support critical systems and higher densities (up to 25kW per cabinet). Standard racks and containment couldn’t fit the existing space or meet reliability and cleanliness requirements.
Solution: CPI delivered a custom cabinet and containment system featuring server cabinets with vertical exhaust ducts and Florida’s first free-standing Hot Aisle Containment (HAC). The HAC was tailored to variable dimensions and included snap-in filler panels and custom cable openings.
Results: “We’re the first data center in the state of Florida to have a free-standing Hot Aisle Containment solution. It maintains cooling while accommodating vendor-supplied storage,” said Joe Keena, Data Center Operations Manager. “Our relationship, the responsiveness of the organization and quality of the product is why we went with CPI,” added the Associate Director of Computer Operations.
Manufacturing Facility: Space-Constrained Deployment
Challenge: IT needed to be deployed on a factory floor with limited space, frequent washdowns, and no HVAC integration. Standard enclosures could not meet space or cooling requirements.
Solution: CPI developed a custom industrial network enclosure with compact footprint, sealed protection, and high-capacity cooling designed specifically for the factory’s conditions.
Results: The custom-built network enclosure allowed the facility to maximize floor space, maintain sanitary conditions, and ensure high-performance cooling without requiring major infrastructure changes.
Why Customization Matters for Operators
Across industries, the value of tailored IT infrastructure is clear:
- Customization protects deployment velocity — projects stay on schedule despite non-standard conditions.
- Customization reduces operational risk — infrastructure fits its environment rather than forcing workarounds.
- Customization extends asset life — by eliminating inefficiencies, operators defer costly facility overhauls.
In today’s climate of AI growth, edge expansion, and compliance pressure, the cost of inaction often exceeds the cost of customization.
Bring Your Vision to Life with CPI
At Chatsworth Products (CPI), customization isn’t an afterthought—it’s our specialty. We don’t just modify standard equipment; we design, engineer, and manufacture solutions that solve complex challenges.
Explore CPI’s full case study library for additional examples, or connect with our team to discuss a project specific to your environment.