For decades, 208V has been the default for rack-level power in U.S. data centers. It was a reasonable choice when server loads were predictable, and cabinet densities left room for inefficiency. AI changes that operating context.
GPU-based systems introduce sustained, high-current draw and far more variability, turning voltage into a practical constraint that affects breaker utilization, physical space, thermal behavior, and how much usable power a rack can support.
While AI infrastructure can still be deployed on 208V, many teams are discovering that practical limits appear earlier than expected, long before facility power is exhausted.
This blog examines where 208V begins to break down under AI workloads and how higher-voltage distribution is reshaping cabinet-level power in GPU-driven environments.
When Voltage Strategy Starts to Matter More Than Power Availability
A growing number of industry leaders, analysts, and technology companies are actively discussing the limitations of legacy 208V power distribution in U.S. data centers—especially as AI workloads and GPU deployments push power density and efficiency requirements far beyond what traditional infrastructure can support.
For most teams, the move away from 208V is not driven by a desire to chase extreme rack densities. It happens gradually, as a series of small constraints begin to accumulate at the cabinet:
- Cabinets creeping toward 30 kW
- Breakers filling faster than expected
- Liquid cooling squeezing rear-of-rack space
- Small changes triggering rework
Over time, these pressures shift the problem from one of raw power availability to one of practical power usability.
At that point, the limiting factor is no longer how much power the facility can supply, but how efficiently—and how precisely—that power can be delivered, distributed, and managed inside the cabinet. Voltage stops being something teams can take for granted and becomes a decision that shapes how the rest of the design scales.
AI does not break 208V outright. It exposes its limits earlier, and it does so at the cabinet level rather than at the facility.
Why 208V Becomes a Constraint in AI Deployments
When teams start talking about power limits, the discussion often centers on kilowatts. In practice, the constraint they encounter first shows up as current.
AI workloads don’t just require more power—they force that power to be delivered at much higher current when lower-voltage distribution is used. At 208V, each increase in power demand translates directly into higher current, driving up resistive losses, conductor size, and breaker utilization.
This is why two deployments with similar kW targets can behave very differently once installed. The difference is not the amount of power being consumed, but how that power is being delivered.
At the same amperage, a three-phase 415V deployment can deliver nearly twice the usable power of a comparable 208V system. Because current—the primary driver of resistive loss—remains constant, the higher-voltage system achieves substantially greater usable capacity.
Why 240V/415V is Becoming the Standard for AI Infrastructure
Attribute | 208V | 240/415V |
|---|---|---|
Voltage Type | Lower voltage (higher current) | Higher voltage (lower current) |
Efficiency | Higher Losses | Lower losses |
Cable Thickness | Larger cables required | Smaller conductors |
Heat Generation | More heat, greater airflow demand | Lower thermal output |
Rack Density | Limited at higher loads | Scalable for AI workloads |
As AI systems move from the 20–30 kW range into sustained 40–50 kW operation and beyond, the limitations of lower-voltage distribution become harder to ignore. For this reason, 240/415V distribution is increasingly recommended for AI deployments. Lower current means lower losses, more efficient use of electrical infrastructure, and greater headroom as workloads scale.
In that context, voltage strategy becomes a practical decision about whether power delivery can keep up with compute—or hold it back. Currently, there are limited IT equipment power supplies that can support voltages greater than 250V. In the future, as more power supplies support 277V; 277/480V distribution is also expected to gain prominence.
Why 240/415V Changes Cabinet-Level Design, Not Just Efficiency
As these current-driven constraints begin to surface, voltage choice starts to influence more than electrical efficiency—it determines how much functional headroom remains inside the cabinet itself.
With 240/415V (wye) systems, power is delivered line-to-neutral at 240V. Because the neutral conductor does not need to be broken, PDUs can use single-pole branch breakers rather than the two-pole protection typically required in 208V deployments. That architectural difference has direct implications for how power distribution hardware is packaged and deployed within dense AI racks.
At the cabinet level, higher-voltage distribution enables:
- Lower breaker density within the PDU
- Reduced internal complexity and heat generation
- Narrower PDU form factors without sacrificing capacity
In cabinets where liquid cooling manifolds, rear-door heat exchangers, and dense cabling are already competing for space, these differences start to matter quickly. Voltage choice often determines whether power distribution fits cleanly into the cabinet—or becomes something teams must work around.
These impacts are often underestimated early in design and only become apparent once physical clearances tighten during installation—when corrective changes are most difficult to implement.
Breaker Count and PDU Density at 208V vs. 415V
Factor | 208V | 240/415V |
|---|---|---|
Typical branch breaker | 20A/30A two pole | 20/30A, single pole |
Power delivered per 20A/30A breaker | 3.3kW/5kW | 3.8kW/5.8kW |
Number of breakers required | More | Fewer |
PDU internal complexity | Higher | Lower |
Max. Power in 2.2" PDU width | 28.8kW | 57.6kW |
Impact on cabinet space | Consumes rear-of-rack space | Preserves space for cooling and cabling |
Max. Power for Similar Amperage Circuits
Amperage | 208V | 240/415V |
|---|---|---|
20A | 5.7kW | 11.5 kW |
30A | 8.6 kW | 17.2 kW |
60A | 17.2 kW | 34.5 kW |
100A | 28.8 kW | 57.6 kW |
Phase Balancing Starts—and Matters—at the Cabinet
As voltage and breaker strategies evolve, phase balancing emerges as the next cabinet-level constraint.
Phase imbalance is often thought of as something that happens upstream in the electrical system, but in AI environments it usually starts right in the rack. GPU workloads are highly variable, and if power isn’t intentionally distributed across phases within the cabinet, it doesn’t take long for one phase to get overloaded while others sit underutilized. When that happens, the effects don’t stay local—they work their way upstream, reducing efficiency, triggering nuisance trips, and leaving usable capacity stranded.
Delivering three-phase power directly to the cabinet makes it possible to balance loads where they actually occur. When power is spread evenly across all three phases within the rack, upstream systems behave more predictably, and operators have a clearer picture of how power is really being used, rather than relying on room-level averages that mask cabinet-specific issues.
At higher cabinet densities, phase balancing stops being a design formality and becomes a requirement for keeping the environment stable.
Power Distribution That Scales with AI
At Chatsworth Products, this shift is reflected in how our eConnect® PDUs are engineered—supporting 240/415V three-phase power, higher-amperage branch protection, and slim form factors designed to coexist with dense, cooling-intensive cabinet layouts.
Beyond raw power delivery, eConnect PDUs provide visibility and control at the cabinet and outlet level. As power consumption becomes more variable and more costly, understanding how power is being used becomes essential to avoiding stranded capacity and unnecessary over-provisioning.
Taken together, these capabilities are designed to support AI deployments as they exist today—and as they continue to scale.
How eConnect® PDUs Support AI Deployments
Deployment Challenge | How CPI Addresses It |
|---|---|
208V power limits capacity at higher AI densities | PDUs designed to support 240/415V 3-phase power distribution supports 2x power densities |
High current increases heat, losses, and stranded capacity. | 240/415V distribution keeps current draws lower resulting in lower losses and higher efficiency |
Limited space inside dense AI cabinets. | Slim 2.2-inch PDU form factors preserve space for liquid cooling hardware and cabling. |
Risk of phase imbalance under variable GPU loads. | Per-outlet and per-phase monitoring enables load balancing and more stable operation. |
20A circuit breakers limits the number of power supplies into a breaker | 30A branch protection provides more flexibility and headroom when plugging GPU power supplies |
See how eConnect® PDUs enable higher-voltage power distribution, and explore AI and HPC infrastructure solutions built to support high-density compute, advanced cooling, and evolving data center demands.