The below software supports a variety of CPI's power and electronic products. Select the appropriate software link below. For assistance please contact our Technical Support Team. Software for eConnect Power Distribution Units eConnect® Power Distribution Unit (PDU) File Release Date Notes Firmware 5.3.1054 07-07-2023 Use only with individual eConnect units with eConnect® Controller 4 (MCM4). This firmware revision is intended for individual eConnect PDUs with an eConnect Controller 4 (MCM4) and can be used in a Secure Array with eConnects that have eConnect Controller 3 (MCM3 controller) or eConnect Controller 2 (MCM2 controller) after those controllers are updated to firmware revision 4.11.731 or later. PDUs with this firmware revision cannot be used in Secure Array with PDUs that have an eConnect Controller 1 (MCM1 controller). Please read Release Notes for details. Firmware 4.13.1054 07-07-2023 Use only with individual eConnect units with MCM3 or MCM2 controller; or if all units within Secure Array® have MCM3 or MCM2 controllers.This firmware revision is intended for individual eConnect PDUs with an eConnect Controller 3 (MCM3 controller) or eConnect Controller 2 (MCM2 controller) or eConnect PDUs within a Secure Array®, all of which have an MCM3 or MCM2 controller. Do not use this firmware version, if any of the PDUs within the Secure Array have an eConnect Controller 1 (MCM1 controller). Please read Release Notes for details Zero Touch Provisioning User Guide 07-29-2020 Use only with eConnect units with eConnect Controller 4 (MCM4) and firmware revision 5.2.757 or later. Command Line Interface User Guide 07-07-2023 Use only with eConnect units with eConnect Controller 4 (MCM4); or with eConnect units with eConnect Controller 3 (MCM3) and firmware revision 4.12.757 or later. Requires a serial console cord to connect a computer to the PDU. See guide for recommendations. Order the serial console cord separately. RESTful API User Guide 07-07-2023 SNMP MIB File 07-07-2023 Software for Networked RFID Electronic Lock Kit Networked RFID Electronic Lock Kit File Release Date Manual / Notes Firmware 5.3.1054 07-07-2023 Please read Release Notes for details. Command Line Interface User Guide 07-07-2023 Use only with Networked RFID Electronic Lock Kits and eConnect units with eConnect Controller 4 (MCM4). Requires a serial console cord to connect a computer to the Networked RFID Electronic Lock Kit. See guide for recommendations. Order the serial console cord separately. SNMP MIB File 07-07-2023 Software for Networked Electronic Access Control (EAC) Networked Electronic Access Control (EAC) File Release Date Manual / Notes Firmware 4.13.1054 07-07-2023 Please read Release Notes for details Command Line Interface User Guide 07-07-2023 Use only with Networked Electronic Access Control (EAC) Kits or eConnect units with eConnect Controller 3 (MCM3) and firmware revision 4.12.757 or later. Requires a serial console cord to connect a computer to the Networked Electronic Access Control (EAC) Kit. See guide for recommendations. Order the serial console cord separately. SNMP MIB File 07-07-2023 Software for other Power Distribution Units Additional Power Distribution Units File Release Date Used with these products MIB Files 1-21-2013 P/N 356XX- and 358XX-series Monitored and Controlled PDUs Serial Access Program* 10-25-2010 P/N 356XX- and 358XX-series Monitored and Controlled PDUs Software for Uninterruptible Power Supplies Uninterruptible Power Supplies File Release Date Used with these products Firmware 3.8.DA806 05/09/2022 UPS’s with SNMP1 – Internal SNMP/Web Card MIB Files 05/09/2022 UPS’s with SNMP1 for DCIM integration Netility Software 05/09/2022 UPS’s with SNMP1 for IP Setup and Search, Firmware Upgrades Shutdown Wizard Contact Tech Support to Obtain File 05/09/2022 Windows servers connected to UPS’s with SNMP1 for Graceful shutdown Software for Remote Infrastructure Management (RIM) Remote Infrastructure Management (RIM) File Release Date Used with these products RIM-1000 Firmware ** 01-19-2023 RIM-1000 RIM-1000 MIB 01-19-2023 RIM-1000 RIM-750 Firmware 9-26-2022 RIM-750 Protocol Converter Firmware 01-19-2023 RIM Protocol Converter Protocol Converter MIB 01-19-2023 RIM Protocol Converter *Serial Software allows you to access, configure, monitor and control select PDUs using a direct serial connection to a computer. Use the RJ-45 to DB-9 Serial Setup Cable (P/N 35941-131) to connect the PDU and computer. Note that PDUs manufactured after September 1, 2009 can be configured using a java-enabled web browser instead of the serial setup. **Please contact Technical Support at 800-834-4969 prior to installing the RIM-1000 Firmware.