As industries grow more data-reliant and digital infrastructure expands, the pressure to scale sustainably has never been greater. Data centers are now central to everything from AI development to global communications—but their environmental impact is drawing increased scrutiny from regulators, investors, and customers alike.
With mounting regulations targeting energy consumption, emissions, and resource efficiency, it’s no longer enough to focus on uptime and performance alone. Environmental compliance has become a defining factor in data center strategy—and the most successful organizations are integrating sustainability directly into infrastructure planning.
At the heart of this shift is smarter capacity planning: the ability to design and scale your infrastructure with environmental responsibility in mind.
The Green Regulation Wave is Here
Environmental regulations are evolving rapidly, reshaping how data centers operate. From international trade policies to regional energy efficiency mandates, new rules are emerging to curb emissions, improve transparency, and accelerate the transition to more sustainable infrastructure.
Some of the most impactful developments include:
- Carbon Border Adjustment Mechanism (CBAM): A policy that places a carbon price on imported goods based on their production emissions. This will influence where and how infrastructure components are sourced and manufactured.
- Energy usage and emissions standards: Regulations like California Title 24 and the EU Energy Efficiency Directive are pushing for reduced data center energy use, real-time monitoring, and documented reductions in greenhouse gas emissions.
- Environmental, Social, and Governance (ESG) requirements: Investors, stakeholders, and customers are demanding greater transparency and performance around sustainability metrics—including PUE (Power Usage Effectiveness) and water usage effectiveness (WUE).
These regulatory pressures introduce new risks—but they also create an opportunity to build infrastructure that is not only compliant, but genuinely efficient, scalable, and future-ready.
Avoiding the Hidden Costs of Falling Behind
When organizations delay sustainability planning, they often face serious challenges down the line:
- Retrofits to cooling or power systems to meet efficiency standards can be disruptive and expensive
- Fines or delays stemming from failed environmental audits or misalignment with new compliance rules
- Lost competitive edge as customers and partners seek greener alternatives
- Over-provisioning, which leads to wasted resources, unused capacity, and higher operational carbon footprints
Proactive infrastructure decisions not only reduce total cost of ownership—they position your business to benefit from government incentives for green technologies and from growing demand for sustainable IT services.
Why Sustainable Capacity Planning is Key
When approached strategically, capacity planning becomes a powerful tool for environmental compliance and long-term efficiency. It allows organizations to:
- Design for efficient power and cooling: Supporting high-density workloads without overtaxing HVAC systems or wasting energy
- Build modularly: Reducing material waste and enabling upgrades without full system overhauls
- Monitor and optimize continuously: With intelligent power and thermal management, teams can track resource use in real time—and course-correct proactively
By embedding sustainability into infrastructure design, organizations avoid the high costs of last-minute retrofits or noncompliance—and lay the groundwork for consistent, measurable environmental performance.
How CPI Helps Customers Meet Sustainability Goals
Chatsworth Products (CPI) is committed to helping data center operators and IT teams design infrastructure that aligns with both performance goals and environmental responsibility. Our approach to capacity planning emphasizes energy efficiency, modular design, and compliance support—enabling organizations to scale sustainably.
Here’s how:
1. Unlock Cooling Efficiency Without Overhauling Your Facility
When cooling is inefficient at the cabinet level, energy waste skyrockets—and so do your costs and emissions. By using airflow containment strategies, data centers can optimize cooling, lower energy consumption while maintaining high-density compute environments.
CPI’s ZetaFrame® Cabinet System gives you precise control over airflow and thermal management at the cabinet level, serving as the foundation for advanced, sustainable cooling strategies.
Integrated with waterless, two-phase, direct-to-chip liquid cooling and optimized for advanced airflow management, ZetaFrame is a high-efficiency, closed-loop solution capable of supporting rack densities of 30 kW and beyond—without the need for traditional water loops or chilled infrastructure.
Here’s how it works:
- Two-phase direct-to-chip cooling targets the hottest components (CPUs and GPUs) at the source, absorbing heat through a sealed evaporative process that uses less power.
- The remaining heat in the cabinet is efficiently managed through air containment—lowering the total energy required for cooling across your facility.
This solution is a powerful, scalable, and environmentally friendly way to manage thermal loads, especially in space-constrained or legacy environments where traditional upgrades are costly or impractical.
2. Intelligent Power Distribution and Environmental Monitoring
Meeting sustainability goals starts with visibility. Track energy usage, environmental conditions, and efficiency metrics at the outlet level—giving you the proof and visibility needed to meet sustainability mandates.
CPI’s eConnect® PDUs deliver outlet-level power metering, environmental monitoring, and remote management—giving customers the data they need to track energy use, manage heat loads, and demonstrate regulatory compliance in real time.
With advanced reporting and secure remote management, you can:
- Identify inefficiencies and wasted energy down to the device level
- Balance thermal loads across cabinets to reduce cooling demand
- Prove compliance with ESG metrics, energy efficiency standards, and regulatory mandates
Whether you’re tracking PUE, carbon output, or equipment-level power draw, eConnect® PDUs give you the tools to monitor what matters—and the insight to optimize for both performance and sustainability.
3. Reduce Packaging Waste with Smarter Infrastructure
Traditional cabinet builds often require separate sourcing, on-site assembly, and significant packaging waste—all of which add time, cost, and environmental impact.
CPI’s integrated cabinet solutions arrive preinstalled with power distribution, cable management, and airflow containment already in place—reducing packaging materials, eliminating excess pallets, and minimizing installation waste. Our integrated cable management, power, and containment solutions are designed for long-term use and easy adaptation—minimizing the need for replacements and reducing e-waste over time. As sustainability standards evolve, modular systems make it easier to remain compliant without costly rebuilds.
Our modular cabinet design makes it easy to adapt your infrastructure as standards evolve—without the need for full cabinet replacements or equipment disposal. This supports a more circular, low-waste approach to infrastructure that aligns with sustainability and cost-saving goals.
4. Go Green From the Ground Up with Compliant, Local Manufacturing
Sustainability and compliance go hand-in-hand—and CPI helps you check both boxes. Our products are engineered and manufactured to meet stringent environmental and sourcing standards, including:
- BABA (Build America, Buy America) and TAA (Trade Agreements Act) for U.S. federal procurement
- EU CE, RoHS, and REACH for global environmental and material safety standards
- Regional production that shortens supply chains, reduces carbon emissions from shipping, and supports local economies
From material traceability to support with compliance documentation, CPI helps ensure your infrastructure investment is responsibly made and globally ready.
CPI’s products are engineered to meet U.S. federal requirements (including BABA and TAA), EU compliance, and global energy efficiency standards. Our domestic and international manufacturing footprint helps reduce emissions associated with long-distance shipping while supporting local economies,
Learn more about how CPI supports regulatory compliance >
Planning for a Greener, Compliant Future
Infrastructure decisions made today will shape not only your data center’s scalability—but its environmental footprint and compliance readiness for years to come.
With smarter capacity planning and sustainable design principles, your organization can stay ahead of regulatory pressures, avoid wasteful overbuilding, and ensure your infrastructure evolves responsibly alongside your business.
Whether you’re preparing for CBAM, optimizing for PUE, or pursuing ESG targets, CPI provides the solutions and support to help you stay green under pressure.
Ready to build a more sustainable data center?
Download our checklist for future-ready capacity planning. Or connect with a CPI expert to start designing an infrastructure strategy that meets your performance and environmental goals.